This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
https://www.iar.com/iar-embedded-workbench/partners/texas-instruments/ti-wireless/
IAR Embedded Workbench with its integrated IAR C/C++ Compiler and C-SPY Debugger is the natural choice for wireless applications. In addition, IAR Systems offers a complete solution of RTOS and middleware components such as TCP/IP and USB that can enhance your embedded design.
Regardless of your selected target microcontroller, IAR Embedded Workbench ensures low memory footprint as well as code portability.
| Device/Platform | Protocol stacks | Development tools |
| CC3200 | Wi-Fi | IAR Embedded Workbench for ARM |
| CC2650 (superset of CC26x0) | IAR Embedded Workbench for ARM | |
| CC2640 | Bluetooth® Smart Bluetooth low energy |
IAR Embedded Workbench for ARM |
| CC2630 | IEEE 802.15.4 ZigBee 6LoWPAN RF4CE |
IAR Embedded Workbench for ARM |
| CC2538 | IEEE 802.15.4 ZigBee 6LoWPAN |
IAR Embedded Workbench for ARM |
| CC2430, CC2431, CC2530, CC2531, CC2533 | ZigBee® RF4CE IEEE 802.15.4 |
IAR Embedded Workbench for 8051 |
| CC2520/CC2420 + MSP430 |
ZigBee IEEE 802.15.4 |
IAR Embedded Workbench for MSP430 |
| CC1110/CC1111 and CC2510/CC2511 | SimpliciTI™ | IAR Embedded Workbench for 8051 |
| MSP430FG4618/F2013 Experimenter Board eZ430-RF2500 Development Tool |
IAR Embedded Workbench for MSP430 | |
| CC2540 CC2541 |
Bluetooth low energy | IAR Embedded Workbench for 8051 |
The following evaluation editions are available for Low Power Wireless solutions from Texas Instruments:















(Version 6.10.2,
197.82 MB)