我想每次P1.6上升沿中断,读取P1.7脚位的状态,OSAL有没有相应的函数还是,开一个函数,像这样设置:
P0INP|=0x1<<6;
PICTL &=~(0x1<<2);
EA=0x1;
IEN2|=(0x1<<4);
P1IFG |=0;
P1DIR &=~(1<<7);
然后写中断函数
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想每次P1.6上升沿中断,读取P1.7脚位的状态,OSAL有没有相应的函数还是,开一个函数,像这样设置:
P0INP|=0x1<<6;
PICTL &=~(0x1<<2);
EA=0x1;
IEN2|=(0x1<<4);
P1IFG |=0;
P1DIR &=~(1<<7);
然后写中断函数
没有直接的函数,可以自己写外部中断的初始化和中断函数.
外部中断的一个完整例子
#include <ioCC2540.h>
#define RLED P1_0
#define led2 P1_1
#define uchar unsigned char
#define uint unsigned int
/*****************************************
//函数声明
*****************************************/
void Delay(uint n);
/*****************************************
//io及LED初始化
*****************************************/
void Init_IO_AND_LED(void)
{
P1DIR = 0X03; //0为输入(默认),1为输入
RLED = 1;
led2 = 1;
P0INP &= ~0X0c;//有上拉、下拉
P1INP &= ~0X40; //选择上拉
P0IEN |= 0X30; //P04 P05
PICTL |= 0X02; //下降沿
EA = 1;
IEN1 |= 0X20; // P0IE = 1;
P0IFG |= 0x00; //P12 P13
};
/*****************************************
//主函数
*****************************************/
void main(void)
{
Init_IO_AND_LED();
while(1)
{
};
}
/*****************************************
//延时
*****************************************/
void Delay(uint n)
{
uint ii;
for(ii=0;ii<n;ii++);
for(ii=0;ii<n;ii++);
for(ii=0;ii<n;ii++);
for(ii=0;ii<n;ii++);
for(ii=0;ii<n;ii++);
}
#pragma vector = P1INT_VECTOR
__interrupt void P1_ISR(void)
{
if(P0IFG>0) //按键中断
{
P0IFG = 0;
RLED = !RLED;
}
P0IF = 0; //清中断标志
}