This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540蓝牙FCC 定频测试: FCC ETSI Test

Other Parts Discussed in Thread: CC2540

大家好!我按照TI官方的FCC ETSI Test

http://processors.wiki.ti.com/index.php/FCC_ETSI_Test

加入如下代码:

uint8_t initialAdvertEnable = FALSE;

SK_Keys |= SK_KEY_LEFT;
   testMode++;
   HalLedSet( HAL_LED_1, HAL_LED_MODE_ON );
   switch(testMode)
   {
   case 1:
     { 
       //1st Push: TX CW, 2402 MHz, 0 dBm 
       HCI_EXT_ModemTestTxCmd(HCI_EXT_TX_UNMODULATED_CARRIER,0);
     }
     break;
   case 2:
     {  
       HCI_EXT_EndModemTestCmd();
       //2nd Push: TX CW, 2440 MHz, 0 dBm 
       HCI_EXT_ModemTestTxCmd(HCI_EXT_TX_UNMODULATED_CARRIER,19);
     }
     break;
   case 3:
     {  
       HCI_EXT_EndModemTestCmd();
       //3rd Push: TX CW, 2480 MHz, 0 dBm 
       HCI_EXT_ModemTestTxCmd(HCI_EXT_TX_UNMODULATED_CARRIER,39);
     }
     break;
}
问题一:为什么我把uint8 initial_advertising_enable = FALSE;不做其他改动,用packet Sniffer抓包工具抓包还是有数据抓到?

   问题二:首先把uint8 initial_advertising_enable = FALSE;然后加入

HCI_EXT_ModemTestTxCmd(HCI_EXT_TX_UNMODULATED_CARRIER,19);
用packet Sniffer抓包抓不到对应channel 19的定频测试数据包;
问题三:官方的FCC ETSI Test加入后,怎么才能验证FCC定频功能是否已经加入成功?或者说用什么工具验证
FCC ETSI Test定频测试功能?