Other Parts Discussed in Thread: CC2540, CC2640
请教一下,现在我有一款用CC2540做的蓝牙产品在做CE-RED认证,认证机构反馈有一项“Blocking测试”无法通过,原因是读取不到芯片收到的数据包,认证机构使用的是CCdebuger连接目标板,然后再用SmartRF Studio7在电脑上读取,以下是测试机构反馈的原文:
“目前RED只剩下最后一项Blocking未测了,目前这一项需要分包到外部实验室测试,经实验室测试人员评估,这个定频软件不能接收出CMW500综测仪发出的数据包的个数,就不能测试出pmin和PER
简单介绍下Blocking这项测试, 让蓝牙模块与综测仪CMW500建立蓝牙连接, 综测仪定在低信道(2402MHz)发送数据包给蓝牙模块,保持小于10%误包率PER的传输通信,然后在2380MHz和2300MHz打一个给定强度的Blocking信号,看它的误包率会不会超过10%, 同样的测试需要在高信道(2480MHz)测试,比如综测仪发包1000,模块方面需要接收到900以上的数据包才能判断合格,现在这款定频软件不能实现接收综测仪发出的数据包,所以没法完成这项测试”
因此想请教一下CC2540要如何做才能完成该项测试?