This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC2650 内部FLASH操作问题

Other Parts Discussed in Thread: CC2650STK

char input;
UART_Handle uart;
UART_Params uartParams;
uint8_t cQF_Buf[20],cLenth=0;
uint8_t StatusWrite;
// osal_snv_init();
// NVOCOP_initNV(NULL);
//osal_snv_read(BLE_NVID_CSRK, KEYLEN, cQF_Buf);
Board_initUART();
/* Create a UART with data processing off. */
UART_Params_init(&uartParams);
uartParams.writeDataMode = UART_DATA_BINARY;
// uartParams.readTimeout = 20;//
uartParams.readDataMode = UART_DATA_BINARY;
uartParams.readReturnMode = UART_RETURN_FULL;
uartParams.readEcho = UART_ECHO_OFF;
uartParams.baudRate = 9600;
uart = UART_open(Board_UART0, &uartParams);

/* Loop forever echoing */
while (1) {

RxNum = UART_read(uart, &input, 1);
ProRxData(RxNum, (uint8_t)input);
// osal_snv_read(BLE_NVID_CSRK, KEYLEN, cQF_Buf);
cLenth = QF_UartAnalysis(cQF_Buf);
if (cLenth)
{
StatusWrite = osal_snv_write(BLE_NVID_CUST_START, 9, cQF_Buf);
memset(cQF_Buf, 0, 9);
if(StatusWrite==SUCCESS)
osal_snv_read(BLE_NVID_CUST_START, 9, cQF_Buf);
UART_write(uart, cQF_Buf, cLenth);
}


}

这是我串口接收程序,不知道为什么调用osal_snv_write函数不成功,用的是CC2650STK_app修改的