This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F Seconday MAC address

Other Parts Discussed in Thread: CC2640R2F

大家好,

想問一下知不知道可否用程式來設定CC2640R2F 的secondary mac address?

我試過用HCI_EXT_SETBDADDR, 但不成功! 但用Flash programmer 2 來設定是可以的.

謝謝

  • There are no VS HCI commands for configuring the secondary IEEE BDADDR to the CCFG, or likewise enabling the flash protection registers. It's recommended to do this via the ROM serial bootloader interface as there are primitives to write to the CCFG where the BDADDR can be stored.

    Refer to the Bootloader & Device Configuration sections of the CC26x0 TRM SWCU117.