This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540通讯速率提高后,手机不兼容



我们生产的蓝牙读卡器使用如下参数,华为荣耀V8, 华为荣耀V9都可以读卡

#define DEFAULT_DESIRED_MIN_CONN_INTERVAL    8

// Maximum connection interval (units of 1.25ms, 800=1000ms) if automatic parameter update request is enabled

#define DEFAULT_DESIRED_MAX_CONN_INTERVAL    32

// Slave latency to use if automatic parameter update request is enabled

#define DEFAULT_DESIRED_SLAVE_LATENCY        1

// Supervision timeout value (units of 10ms, 1000=10s) if automatic parameter update request is enabled

#define DEFAULT_DESIRED_CONN_TIMEOUT          600

 

但因为我们需要提高蓝牙与手机的通讯速度,就更改到如下参数,发现华为荣耀V8可以读卡, 华为荣耀V9不可以读卡

#define DEFAULT_DESIRED_MIN_CONN_INTERVAL    8

// Maximum connection interval (units of 1.25ms, 800=1000ms) if automatic parameter update request is enabled

#define DEFAULT_DESIRED_MAX_CONN_INTERVAL    16

// Slave latency to use if automatic parameter update request is enabled

#define DEFAULT_DESIRED_SLAVE_LATENCY        0

// Supervision timeout value (units of 10ms, 1000=10s) if automatic parameter update request is enabled

#define DEFAULT_DESIRED_CONN_TIMEOUT          300

附件是LOG文件

 

 

CC2540ISSUE.zip