Other Parts Discussed in Thread: CC2541, CC2640R2F, CC2652R, CC2650
我这边是通过osal_start_timerEx(simpleBLETaskId, LED_FLASH_EVT, 50);启动一个 50ms的 EVT 定时WriteLongCharValue给从模块发送50个字节数据的,固定发送数据个数为10000个字节,发现50ms发送只能收到大概1000个,如果将任务时间周期改为 200ms一上,则就可以正常发送不丢包,我从机与主机通讯间隔最大最小设置为 8,官方不是声称 2K以内传输速率可以稳定不丢包的吗?请问我这种情况是什么原因呢?TI 员工