Other Parts Discussed in Thread: CC2640R2F
扫描窗口和扫描间隔 一致的话,就表示一致扫描,然后再把扫描持续时间改为500ms,在扫描完成的事件中,再次触发扫描,这种情况下,是不是扫描窗口设置 80,240,120 等 是没有区别的呢?对扫描到其他设备影响不大?还是说需要根据从机的广播间隔进行设置,比如从机广播间隔100ms ,设置哪种扫描参数合适呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
scanning windows设置为advertising interval + 10ms
In a time-constrained application, when the user needs to receive the data as fast as possible, make sure that scanning window is more than the advertising interval + 10ms to guarantee discovery. (The 10 ms extra account for the 0 ms to 10 ms of pseudo-random delay in between each advertising event, assuming no interference.) Following this rule will increase the chance of receiving the advertising packet on the first scan.
您好:
我的这两个参数scanning windows advertising interval设置必须一样,要是设置不同的参数,就无法扫描了。这是什么原因啊?
// Scan parameters
#define DEFAULT_SCAN_DURATION 0//0//4000//2000 //mod lhj 190906 // 值越小,则发现的同一设备广播包越多
#define DEFAULT_SCAN_WIND 10 //120 //
#define DEFAULT_SCAN_INT 10 //120
// Discovey mode (limited, general, all)
#define DEFAULT_DISCOVERY_MODE DEVDISC_MODE_ALL //mod lhj 190929 @@@ DEVDISC_MODE_GENERAL
// TRUE to use active scan
#define DEFAULT_DISCOVERY_ACTIVE_SCAN FALSE
// Set desired policy to use during discovery (use values from GAP_Disc_Filter_Policies)
#define DEFAULT_DISCOVERY_WHITE_LIST GAP_DISC_FILTER_POLICY_ALL
// TRUE to use high scan duty cycle when creating link
#define DEFAULT_LINK_HIGH_DUTY_CYCLE FALSE
// TRUE to use white list when creating link
#define DEFAULT_LINK_WHITE_LIST FALSE