This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F 打开调试功能,串口助手收到的是乱码

串口收到的信息

c[2J[10r[11;1H7[10r[1;1H[2KBLE Central87[10r[2;1H[2K0xB0912269F97B87[10r[3;1H[2KInitialized87[10r[6;1H[2KDiscover ->87[10r[3;1H[2K87[10r[4;1H[2K87[10r[6;1H[2KDiscover ->8

  • 你需要使用的putty 才能正常显示。
    此外波特率115200.
    https://www.putty.org/
  • 根本没解决问题.还是出现乱码.
  • 遇到同样的问题,串口打印:
    .c.[2J.[10r.[11;1H.7.[10r.[1;1H.[2KBLE Peripheral.8.7.[10r.[2;1H.[2K0xC464E3ACC862.8.7.[10r.[3;1H.[2KInitialized.8.7.[10r.[3;1H.[2KAdvertising.8.c.[2J.[10r.[11;1H.7.[10r.[1;1H.[2KBLE Peripheral.8.7.[10r.[2;1H.[2K0xC464E3ACC862.8.7.[10r.[3;1H.[2KInitialized.8.7.[10r.[3;1H.[2KAdvertising.8
  • 你有使用的putty 波特率115200嗎?測試的sdk版本跟例程是?
  • 昨天我浏览SDK代码时发现以下代码:

    /* -----------------------------------------------------------------------------
     *  Constants and macros
     * -----------------------------------------------------------------------------
     */
    #ifndef MIN
    #  define MIN(n, m)    (((n) > (m)) ? (m) : (n))
    #endif
    
    #define DISPLAY_UART_ESC_INITIAL            "\x1b\x63"    /* Reset terminal */                \
                                                "\x1b[2J"     /* Clear screen   */                \
                                                "\x1b[10r"    /* Scrolling region from line 10 */ \
                                                "\x1b[11;1H"  /* Set initial cursor to line 11 */
    
    #define DISPLAY_UART_ESC_MOVEPOS_FMT        "\x1b\x37"    /* Save cursor position */ \
                                                "\x1b[10r"    /* Retransmit scroll    */ \
                                                "\x1b[%d;%dH" /* Move cursor fmt str  */
    
    #define DISPLAY_UART_ESC_RESTOREPOS         "\x1b\x38"    /* Restore saved cursor pos */
    
    #define DISPLAY_UART_ESC_CLEAR_SCREEN       "\x1b[2J"     /* Clear screen       */
    #define DISPLAY_UART_ESC_CLEAR_CUR_LEFT     "\x1b[1K"     /* Clear cursor left  */
    #define DISPLAY_UART_ESC_CLEAR_CUR_RIGHT    "\x1b[0K"     /* Clear cursor right */
    #define DISPLAY_UART_ESC_CLEAR_BOTH         "\x1b[2K"     /* Clear line         */
    #define DISPLAY_UART_ESC_CLEARSEQ_LEN       4

    原来这些字符串不是乱码而是VT100终端控制码,因为我使用的终端不支持控制码所以导致出现乱码,后来改用screen命令就不会有乱码了。

    所以和波特率没有关系,换一个支持终端控制码的终端就可以解决这个问题。