This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【CC2541 评测】+ 用安卓手机测试CC2541DK-MINI+by dirtwillfly

Other Parts Discussed in Thread: CC2541DK-MINI, CC2540, CC2541

一、拆箱

收到CC2541DK-MINI有几天了,先晒晒本次评测的主角:

1、包装盒,一如既往的黑红风格

包装盒边沿磨出了白色,显得略微有点旧。

在包装盒的一侧粘贴着评估板的型号和版本:CC2541DK-MINI Revision 1.0.2

2、外壳也是黑红风格。外壳的里面有一侧是红色的,在黑色的外表下,有一个火热的内涵。ti的这个评估板很贴心,另外还带了一个安装外壳的螺丝,螺丝就不贴图了。

3、转接板和排线,一如既往地贴心周到。

4、CC2541Dongle 

版本1.0

上面主要是一颗cc2540,板载PCB天线,电源电路使用的TPS76933。另外有两个按键、两个led,还有调试接口和8个io。需要的时候这个CC2541Dongle 也可以做为一个简单的开发板来使用。

5、正版CC Debugger仿真器

6、本评估套件的核心:

板子正面:板载cc2541、pcb天线、电池座、红绿双色led、两个按键、调试接口和io扩展接口。还有BMA250三轴加速度传感器。

板子背面是一个贴片蜂鸣器,这个蜂鸣器是低功耗的哦。在3Vp-p 4.0kHz方波条件下工作电流最大3mA,声音不小于70dB。

双色led动作很妖娆,屈腿弯腰   ^_^    ^_^

7、全家福,还带包装袋,拍的有点乱。

8、阶段性总结

从上面可以看出,CC2541DK-MINI工具包含了完整的cc2540/cc2541开发工具,可扩展的io、三轴加速度传感器和必要的按键、led等资源。完全能够满足使用该评估套件作为开发自己的蓝牙产品的原型和评估工具。

x 出现错误。请重试或与管理员联系。