This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于cc2640rf bootloader 串口升级问题



你好:

我在使用cc2640rf开发应用,最近我想添加uart升级功能。我按照官方手册配置了cfg:我的配置如下图:

我开启了bootloader,使用DIO:9作用使能脚,低电平使能,开启后门(C5 09 FE C5).

现在问题是,我在将IO9拉低之后,重启设备,我的串口没有输出输出了(正常情况下,我的app是用串口信息输出的),我不确定是否进入了bootloader mode?

另外我还尝试了使用Flash Programmer2 擦除flash,如果没有flash,设备应该能进入bootloader mode才对,但是此时我使用uart0尝试去连接,但是每次都是不能检测到波特率。

我使用github上一个移植官方的uart demo的app,该程序运行正常。我尝试去抓包,发现每次发送55的时候无法设备无返回,每次遇到的错误都是无法检测波特率。

我使用Flash Programmer2下xds100v3,可以连接设备,但是我使用xds的串口尝试连接设备,但是连接不上。

希望得到的帮助:我想知道有哪一步错了