This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2640r2f 配对时,手机端能否不弹出输入密码的界面

我们的SDK版本是:1.35,现在添加了配对加密功能,但每次手机连接时都会弹出输入密码的界面,客户体验不好。

我们希望手机端在连接蓝牙设备端时,不会弹出输入密码的界面,而是在手机端的APP中通过某种方式直接把“密码”传递过来,相当于把输入密码的过程变为隐性传递了。而其它APP(非我方实现)连接时因为没有传递密码,会被设备端认为配对无效。

请问这个功能是需要修改配对的方式吗?我现在的配置如下:

uint8_t pairMode = GAPBOND_PAIRING_MODE_INITIATE;
uint8_t mitm = TRUE;
uint8_t ioCap = GAPBOND_IO_CAP_DISPLAY_ONLY;
uint8_t bonding = FALSE;

我查看ioCap还可以有以下几中选择:

395 /** @defgroup GAPBondMgr_IO_Caps GAP Bond Manager I/O Capabilities
396 * @{
397 */
398 #define GAPBOND_IO_CAP_DISPLAY_ONLY 0x00 //!< Display Only Device
399 #define GAPBOND_IO_CAP_DISPLAY_YES_NO 0x01 //!< Display and Yes and No Capable
400 #define GAPBOND_IO_CAP_KEYBOARD_ONLY 0x02 //!< Keyboard Only
401 #define GAPBOND_IO_CAP_NO_INPUT_NO_OUTPUT 0x03 //!< No Display or Input Device
402 #define GAPBOND_IO_CAP_KEYBOARD_DISPLAY 0x04 //!< Both Keyboard and Display Capable
403 /** @} End GAPBondMgr_IO_Caps */

是否要改为GAPBOND_IO_CAP_KEYBOARD_ONLY?

还有请有相关经验的各位大佬解答一下,谢谢!