This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GPIO_CFG_OUT_STD输出引脚是主动驱动的高和低,主动驱动什么意思?和普通输出引脚有什么区别

 GPIO_CFG_OUT_STD输出引脚是主动驱动的高和低,主动驱动什么意思?和普通输出引脚有什么区别 ?

GPIO_CFG_OUT_STR_LOW 引脚强度设置为低,什么意思?什么时候需要设置引脚强度?

  • #define GPIO_CFG_OUTPUT            (((uint32_t) 0) << GPIO_CFG_IO_LSB) /*!< @hideinitializer Pin is an output. */
    #define GPIO_CFG_OUT_STD           (((uint32_t) 0) << GPIO_CFG_IO_LSB) /*!< @hideinitializer Output pin is actively driven high and low */
    #define GPIO_CFG_OUT_OD_NOPULL     (((uint32_t) 2) << GPIO_CFG_IO_LSB) /*!< @hideinitializer Output pin is Open Drain */
    #define GPIO_CFG_OUT_OD_PU         (((uint32_t) 4) << GPIO_CFG_IO_LSB) /*!< @hideinitializer Output pin is Open Drain w/ pull up */
    #define GPIO_CFG_OUT_OD_PD         (((uint32_t) 6) << GPIO_CFG_IO_LSB) /*!< @hideinitializer Output pin is Open Drain w/ pull dn */
    
    #define GPIO_CFG_OUT_STR_LOW       (((uint32_t) 0) << GPIO_CFG_OUT_STRENGTH_LSB) /*!< @hideinitializer Set output pin strength to low */
    #define GPIO_CFG_OUT_STR_MED       (((uint32_t) 1) << GPIO_CFG_OUT_STRENGTH_LSB) /*!< @hideinitializer Set output pin strength to medium */
    #define GPIO_CFG_OUT_STR_HIGH      (((uint32_t) 2) << GPIO_CFG_OUT_STRENGTH_LSB) /*!< @hideinitializer Set output pin strength to high */
    
    #define GPIO_CFG_OUT_HIGH          (((uint32_t) 1) << GPIO_CFG_OUT_BIT) /*!< @hideinitializer Set pin's output to 1. */
    #define GPIO_CFG_OUT_LOW           (((uint32_t) 0) << GPIO_CFG_OUT_BIT) /*!< @hideinitializer Set pin's output to 0. */

    设置引脚的驱动强度,有些应用需要引脚有高驱动能力