This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2802x Adc采样问题



Adc配置为内部基准参考,查阅手册,电压为3.3V 

AdcRegs.ADCCTL1.bit.ADCREFSEL = 0;      // Select interal BG 0:internal 1:external
 AdcRegs.ADCCTL1.bit.ADCBGPWD = 1;   // Power up band gap Device_cal
 AdcRegs.ADCCTL1.bit.ADCREFPWD = 1;   // Power up reference
 AdcRegs.ADCCTL1.bit.ADCPWDN = 1;   // Power up rest of ADC
 AdcRegs.ADCCTL1.bit.ADCENABLE = 1;   // Enable ADC

采样直流电压0-330Vdc对于进入Adc口的电压为0-3.3V。现在直流设定200V,ADC入口电压2V,采样值应该为4096*2/3.3=2482,但是实际采样为2256,采样值相差10%,

这是为什么,谢谢各位大神