This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc26x2开发板起步探索



  各位大神好,刚开始接触,很多还不太懂,现在遇到了个问题,向各位大神求教~~

在ccs7.4下,载入sdk中的project_zero例程,以下报错是什么意思,该怎么解决?

Description Resource Path Location Type
#1965 cannot open source file "ti_ble_config.h" osal_icall_ble.c /project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs/Startup line 85 C/C++ Problem
#1965 cannot open source file "ti_drivers_config.h" project_zero.c /project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs/Application line 90 C/C++ Problem
#1965 cannot open source file "ti_radio_config.h" ble_user_config.c /project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs/iCallBLE line 62 C/C++ Problem
#1965 cannot open source file "ti_radio_config.h" ble_user_config_stack.c /project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs/Startup line 57 C/C++ Problem
#20 identifier "cteAntProp_t" is undefined .ccsproject /project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs line 142, external location: C:\ti\simplelink_cc13x2_26x2_sdk_3_40_00_02\source\ti\ble5stack\controller\cc26xx\inc\ll_user_config.h C/C++ Problem
#20 identifier "ECCParams_CurveParams" is undefined .ccsproject /project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs line 132, external location: C:\ti\simplelink_cc13x2_26x2_sdk_3_40_00_02\source\ti\ble5stack\controller\cc26xx\inc\ll_user_config.h C/C++ Problem
#20 identifier "rfOpCmd_cntBranch_t" is undefined .ccsproject /project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs line 1147, external location: C:\ti\simplelink_cc13x2_26x2_sdk_3_40_00_02\source\ti\ble5stack\controller\cc26xx\inc\ll_ae.h C/C++ Problem
#20 identifier "rfOpCmd_runImmedCmd_t" is undefined .ccsproject /project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs line 1658, external location: C:\ti\simplelink_cc13x2_26x2_sdk_3_40_00_02\source\ti\ble5stack\controller\cc26xx\inc\ll_common.h C/C++ Problem
#20 identifier "rfOpCmd_runImmedCmd_t" is undefined .ccsproject /project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs line 1660, external location: C:\ti\simplelink_cc13x2_26x2_sdk_3_40_00_02\source\ti\ble5stack\controller\cc26xx\inc\ll_common.h C/C++ Problem
#20 identifier "rtosApiTblPtr_t" is undefined .ccsproject /project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs line 125, external location: C:\ti\simplelink_cc13x2_26x2_sdk_3_40_00_02\source\ti\ble5stack\controller\cc26xx\inc\ll_user_config.h C/C++ Problem
#35 #error directive: flash_interface.h /project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs/OAD line 170 C/C++ Problem
#35 #error directive: Callback Timer module shouldn't be included (no callback timer is needed)! .ccsproject /project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs line 77, external location: C:\ti\simplelink_cc13x2_26x2_sdk_3_40_00_02\source\ti\ble5stack\osal\src\inc\osal_cbtimer.h C/C++ Problem
Cannot open command file 'D:/ti_work/project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs/Debug/syscfg/ti_ble_app_config.opt': No such file or directory null: Cannot open command file 'D:/ti_work/project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs/Debug/syscfg/ti_ble_app_config.opt': No such file or directory project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
Cannot open command file 'D:/ti_work/project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs/Debug/syscfg/ti_build_config.opt': No such file or directory null: Cannot open command file 'D:/ti_work/project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs/Debug/syscfg/ti_build_config.opt': No such file or directory project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: *** [Application/project_zero.obj] Error 1 project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: *** [iCallBLE/ble_user_config.obj] Error 1 project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: *** [OAD/crc32.obj] Error 1 project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: *** [OAD/flash_interface_ext_rtos_NVS.obj] Error 1 project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: *** [OAD/oad.obj] Error 1 project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: *** [Profiles/button_service.obj] Error 1 project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: *** [Profiles/data_service.obj] Error 1 project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: *** [Profiles/devinfoservice.obj] Error 1 project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: *** [Profiles/gattservapp_util.obj] Error 1 project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: *** [Profiles/led_service.obj] Error 1 project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: *** [Startup/ble_user_config_stack.obj] Error 1 project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: *** [Startup/main.obj] Error 1 project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: *** [Startup/osal_icall_ble.obj] Error 1 project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: *** [Startup/rom_init.obj] Error 1 project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem
gmake: Target 'all' not remade because of errors. project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs C/C++ Problem