This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F OAD工程问题

Expert 2040 points
Other Parts Discussed in Thread: CC2640R2F

CC2640R2F OAD 工程编译出现下面的错误

Error[Lp011]: section placement failed
unable to allocate space for sections/blocks with a total estimated minimum size of 0x9e71 bytes (max align 0x4) in <[0x1330-0xafff]> (total uncommitted space 0x9cd0).
Error[Lp017]: the address of "primaryServiceUUID" was needed when computing compressed initializers for section .data (devinfoservice.o #19), but that address hasn't been set yet, since the
size of the compressed initializers are needed in order to set it
Tool Internal Error:
Internal Error: [CoreUtil/General]: Access violation (0xc0000005) at 00E79284 (reading from address 0x14)
Internal Error: [CoreUtil/General]: Access violation (0xc0000005) at 00E79284 (reading from address 0x14)
Error while running Linker