This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用BTOOL工具升级时,总是失败,这是什么原因?麻烦帮我分析下!



cc2642r1  sdk: simplelink_cc13x2_26x2_sdk_3_40_00_02   

设备原有固件:simple_peripheral_oad_onchip

设备新的升级固件:project_zero

在连接成功后,按下send按钮,运行到一定的时候,出现OAD Download Not Successful

log如下:

--------------------------------------------------------------------
[59] : <Rx> - 11:26:59.702
-Type : 0x04 (Event)
-EventCode : 0x00FF (HCI_LE_ExtEvent)
-Data Length : 0x0B (11) bytes(s)
Event : 0x0607 (1543) (GAP_LinkParamUpdate)
Status : 0x00 (0) (SUCCESS)
ConnHandle : 0x0000 (0)
ConnInterval : 0x0006 (6)
ConnLatency : 0x0000 (0)
ConnTimeout : 0x0032 (50)
Dump(Rx):
0000:04 FF 0B 07 06 00 00 00 06 00 00 00 32 00 ............2.
--------------------------------------------------------------------
[60] : <Info> - 11:27:01.207
Device Disconnected
Handle = 0x0000
Addr Type = 0x00 (ADDRTYPE_PUBLIC)
BDAddr = 58:93:D8:A4:B7:05
--------------------------------------------------------------------
[61] : <Rx> - 11:27:01.202
-Type : 0x04 (Event)
-EventCode : 0x00FF (HCI_LE_ExtEvent)
-Data Length : 0x06 (6) bytes(s)
Event : 0x0606 (1542) (GAP_TerminateLink)
Status : 0x00 (0) (SUCCESS)
ConnHandle : 0x0000 (0)
Reason : 0x08 (8) (SUPERVISION_TIMEOUT_TERM)
Dump(Rx):
0000:04 FF 06 06 06 00 00 00 08 .........
--------------------------------------------------------------------
[62] : <Info> - 11:27:12.721
Establish Connection
--------------------------------------------------------------------
[63] : <Tx> - 11:27:12.724
-Type : 0x01 (Command)
-OpCode : 0xFE62 (GapInit_connect)
-Data Length : 0x0A (10) byte(s)
PeerAddrType : 0x00 (0) (PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID)
PeerAddr : 58:93:D8:A4:B7:05
InitiatingPhy : 0x01 (1) (
INIT_PHY_1M)
Timeout : 0x0000 (0)
Dump(Tx):
0000:01 62 FE 0A 00 05 B7 A4 D8 93 58 01 00 00 .b........X...
--------------------------------------------------------------------
[64] : <Rx> - 11:27:12.749
-Type : 0x04 (Event)
-EventCode : 0x00FF (HCI_LE_ExtEvent)
-Data Length : 0x06 (6) bytes(s)
Event : 0x067F (1663) (GAP_HCI_ExtentionCommandStatus)
Status : 0x00 (0) (SUCCESS)
OpCode : 0xFE62 (GapInit_connect)
DataLength : 0x00 (0)
Dump(Rx):
0000:04 FF 06 7F 06 00 62 FE 00 ......b..
--------------------------------------------------------------------
[65] : <Rx> - 11:27:12.819
-Type : 0x04 (Event)
-EventCode : 0x00FF (HCI_LE_ExtEvent)
-Data Length : 0x14 (20) bytes(s)
Event : 0x0605 (1541) (GAP_EstablishLink)
Status : 0x00 (0) (SUCCESS)
DevAddrType : 0x00 (0) (ADDRTYPE_PUBLIC)
DevAddr : 58:93:D8:A4:B7:05
ConnHandle : 0x0000 (0)
ConnRole : 0x08 (8) (
Central)
ConnInterval : 0x0050 (80)
ConnLatency : 0x0000 (0)
ConnTimeout : 0x07D0 (2000)
ClockAccuracy : 0x00 (0)
Dump(Rx):
0000:04 FF 14 05 06 00 00 05 B7 A4 D8 93 58 00 00 08 ............X...
0010:50 00 00 00 D0 07 00 P......
--------------------------------------------------------------------
[66] : <Tx> - 11:27:12.820
-Type : 0x01 (Command)
-OpCode : 0x2022 (HCI_LE_SetDataLength)
-Data Length : 0x06 (6) byte(s)
Handle : 0x0000 (0)
TxOctets : 0x00FB (251)
TxTime : 0x0848 (2120)
Dump(Tx):
0000:01 22 20 06 00 00 FB 00 48 08 ." .....H.
--------------------------------------------------------------------
[67] : <Info> - 11:27:12.855
Device Connected
Handle = 0x0000
Addr Type = 0x00 (ADDRTYPE_PUBLIC)
BDAddr = 58:93:D8:A4:B7:05
--------------------------------------------------------------------
[68] : <Rx> - 11:27:12.849
-Type : 0x04 (Event)
-EventCode : 0x000E (HCI_CommandCompleteEvent)
-Data Length : 0x06 (6) bytes(s)
Packets : 0x01 (1)
OpCode : 0x2022 (HCI_LE_SetDataLength)
Status : 0x00 (0) (SUCCESS)
Handle : 0x0000 (0)
Dump(Rx):
0000:04 0E 06 01 22 20 00 00 00 ...." ...
--------------------------------------------------------------------
[69] : <Info> - 11:27:12.869
Restore Connection Parameters
--------------------------------------------------------------------
[70] : <Info> - 11:27:12.884
Image Service Discovery
--------------------------------------------------------------------
[71] : <Info> - 11:27:12.887
Image Service Discovery
--------------------------------------------------------------------
[72] : <Tx> - 11:27:12.870
-Type : 0x01 (Command)
-OpCode : 0x2016 (HCI_LEReadRemoteUsedFeatures)
-Data Length : 0x02 (2) byte(s)
Handle : 0x0000 (0)
Dump(Tx):
0000:01 16 20 02 00 00 .. ...
--------------------------------------------------------------------
[73] : <Info> - 11:27:12.893
OAD Send UUID Discovery
--------------------------------------------------------------------
[74] : <Tx> - 11:27:12.895
-Type : 0x01 (Command)
-OpCode : 0xFD86 (GATT_DiscPrimaryServiceByUUID)
-Data Length : 0x12 (18) byte(s)
ConnHandle : 0x0000 (0)
Value : 00:00:00:00:00:00:00:B0:00:40:51:04:C0:FF:00:F0
Dump(Tx):
0000:01 86 FD 12 00 00 00 00 00 00 00 00 00 B0 00 40 ...............@
0010:51 04 C0 FF 00 F0 Q.....
--------------------------------------------------------------------
[75] : <Rx> - 11:27:12.929
-Type : 0x04 (Event)
-EventCode : 0x00FF (HCI_LE_ExtEvent)
-Data Length : 0x06 (6) bytes(s)
Event : 0x067F (1663) (GAP_HCI_ExtentionCommandStatus)
Status : 0x00 (0) (SUCCESS)
OpCode : 0xFD86 (GATT_DiscPrimaryServiceByUUID)
DataLength : 0x00 (0)
Dump(Rx):
0000:04 FF 06 7F 06 00 86 FD 00 .........
--------------------------------------------------------------------
[76] : <Rx> - 11:27:13.119
-Type : 0x04 (Event)
-EventCode : 0x003E (HCI_LE_GenericReportEvent)
-Data Length : 0x0C (12) bytes(s)
LE Event Code : 0x04 (4) (HCI_LE_ReadRemoteUsedFeaturesCompleteEvent)
LE Event Code : 0x04 (4) (HCI_LE_ReadRemoteUsedFeaturesCompleteEvent)
Status : 0x00 (0) (SUCCESS)
ConnectionId : 0x0000 (0)
Features : 0x00000000000059FF (23039) (
Encryption
Connection_Parameters_Request
Reject_Extended_Indication
Slave_Features_Exchange
Ping
Data_Packet_Length_Extension
Privacy
Extended_Scanner_Filter_Policies
PHY_2M
Coded_PHY
Extended_Advertising
Channel_Selection_Algorithm_2)
Dump(Rx):
0000:04 3E 0C 04 00 00 00 FF 59 00 00 00 00 00 00 .>......Y......
--------------------------------------------------------------------
[77] : <Rx> - 11:27:13.219
-Type : 0x04 (Event)
-EventCode : 0x00FF (HCI_LE_ExtEvent)
-Data Length : 0x0A (10) bytes(s)
Event : 0x0501 (1281) (ATT_ErrorRsp)
Status : 0x00 (0) (SUCCESS)
ConnHandle : 0x0000 (0)
PduLen : 0x04 (4)
ReqOpCode : 0x06 (ATT_FindByTypeValueReq)
Handle : 0x0001 (1)
ErrorCode : 0x0A (10) (ATTR_NOT_FOUND)
Dump(Rx):
0000:04 FF 0A 01 05 00 00 00 04 06 01 00 0A .............
--------------------------------------------------------------------
[78] : <Info> - 11:27:13.239
OAD - Restore Connection Settings
--------------------------------------------------------------------
[79] : <Error> - 11:27:13.241
OAD Download Not Successful
--------------------------------------------------------------------
[80] : <Tx> - 11:27:13.226
-Type : 0x01 (Command)
-OpCode : 0xFE11 (GAP_UpdateLinkParamReq)
-Data Length : 0x0A (10) byte(s)
ConnHandle : 0x0000 (0)
IntervalMin : 0x0006 (6)
IntervalMax : 0x0006 (6)
ConnLatency : 0x0000 (0)
ConnTimeout : 0x0032 (50)
Dump(Tx):
0000:01 11 FE 0A 00 00 06 00 06 00 00 00 32 00 ............2.
--------------------------------------------------------------------
[81] : <Tx> - 11:27:13.243
-Type : 0x01 (Command)
-OpCode : 0x2016 (HCI_LEReadRemoteUsedFeatures)
-Data Length : 0x02 (2) byte(s)
Handle : 0x0000 (0)
Dump(Tx):
0000:01 16 20 02 00 00 .. ...
--------------------------------------------------------------------
[82] : <Rx> - 11:27:13.269
-Type : 0x04 (Event)
-EventCode : 0x00FF (HCI_LE_ExtEvent)
-Data Length : 0x06 (6) bytes(s)
Event : 0x067F (1663) (GAP_HCI_ExtentionCommandStatus)
Status : 0x00 (0) (SUCCESS)
OpCode : 0xFE11 (GAP_UpdateLinkParamReq)
DataLength : 0x00 (0)
Dump(Rx):
0000:04 FF 06 7F 06 00 11 FE 00 .........
--------------------------------------------------------------------
[83] : <Rx> - 11:27:13.280
-Type : 0x04 (Event)
-EventCode : 0x003E (HCI_LE_GenericReportEvent)
-Data Length : 0x0C (12) bytes(s)
LE Event Code : 0x04 (4) (HCI_LE_ReadRemoteUsedFeaturesCompleteEvent)
LE Event Code : 0x04 (4) (HCI_LE_ReadRemoteUsedFeaturesCompleteEvent)
Status : 0x00 (0) (SUCCESS)
ConnectionId : 0x0000 (0)
Features : 0x00000000000059FF (23039) (
Encryption
Connection_Parameters_Request
Reject_Extended_Indication
Slave_Features_Exchange
Ping
Data_Packet_Length_Extension
Privacy
Extended_Scanner_Filter_Policies
PHY_2M
Coded_PHY
Extended_Advertising
Channel_Selection_Algorithm_2)
Dump(Rx):
0000:04 3E 0C 04 00 00 00 FF 59 00 00 00 00 00 00 .>......Y......
--------------------------------------------------------------------
[84] : <Tx> - 11:27:13.280
-Type : 0x01 (Command)
-OpCode : 0xFE11 (GAP_UpdateLinkParamReq)
-Data Length : 0x0A (10) byte(s)
ConnHandle : 0x0000 (0)
IntervalMin : 0x0050 (80)
IntervalMax : 0x0050 (80)
ConnLatency : 0x0000 (0)
ConnTimeout : 0x07D0 (2000)
Dump(Tx):
0000:01 11 FE 0A 00 00 50 00 50 00 00 00 D0 07 ......P.P.....
--------------------------------------------------------------------
[85] : <Rx> - 11:27:13.319
-Type : 0x04 (Event)
-EventCode : 0x00FF (HCI_LE_ExtEvent)
-Data Length : 0x06 (6) bytes(s)
Event : 0x067F (1663) (GAP_HCI_ExtentionCommandStatus)
Status : 0x00 (0) (SUCCESS)
OpCode : 0xFE11 (GAP_UpdateLinkParamReq)
DataLength : 0x00 (0)
Dump(Rx):
0000:04 FF 06 7F 06 00 11 FE 00 .........
--------------------------------------------------------------------
[86] : <Rx> - 11:27:14.819
-Type : 0x04 (Event)
-EventCode : 0x00FF (HCI_LE_ExtEvent)
-Data Length : 0x0B (11) bytes(s)
Event : 0x0607 (1543) (GAP_LinkParamUpdate)
Status : 0x00 (0) (SUCCESS)
ConnHandle : 0x0000 (0)
ConnInterval : 0x0006 (6)
ConnLatency : 0x0000 (0)
ConnTimeout : 0x0032 (50)
Dump(Rx):
0000:04 FF 0B 07 06 00 00 00 06 00 00 00 32 00 ............2.
--------------------------------------------------------------------
[87] : <Rx> - 11:27:18.836
-Type : 0x04 (Event)
-EventCode : 0x000E (HCI_CommandCompleteEvent)
-Data Length : 0x06 (6) bytes(s)
Packets : 0x01 (1)
OpCode : 0x2020 (HCI_LE_RemoteConnectionParameterRequestReply)
Status : 0x00 (0) (SUCCESS)
Handle : 0x0000 (0)
Dump(Rx):
0000:04 0E 06 01 20 20 00 00 00 .... ...
--------------------------------------------------------------------
[88] : <Rx> - 11:27:18.926
-Type : 0x04 (Event)
-EventCode : 0x00FF (HCI_LE_ExtEvent)
-Data Length : 0x0B (11) bytes(s)
Event : 0x0607 (1543) (GAP_LinkParamUpdate)
Status : 0x00 (0) (SUCCESS)
ConnHandle : 0x0000 (0)
ConnInterval : 0x0320 (800)
ConnLatency : 0x0000 (0)
ConnTimeout : 0x0258 (600)
Dump(Rx):
0000:04 FF 0B 07 06 00 00 00 20 03 00 00 58 02 ........ ...X.
--------------------------------------------------------------------