This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTLS AOA指定信道

想指定slave/passive/master 只在單一信道量測IQ,請問要如何設定

  • 可以修改为特定信道Note that the same data (ADV_IND) is sent on all three channels. Since the packet is quite small (remember that the advertisement data is no more than 31 bytes), it takes less than 10 ms to send it. The device can be modified to advertise only on selected channels.
    操作请看这边:
    Advertising Task 1 – Change Advertising Parameters
    dev.ti.com/.../node