This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2640蓝牙模块断电,主机要20s很久才能发现从机断连了

哪个参数和设置从机连接参数有关?

感觉蓝牙连接参数好像没有配进去

// HID idle timeout in msec; set to zero to disable timeout
#define DEFAULT_HID_IDLE_TIMEOUT 60000

// Minimum connection interval (units of 1.25ms) if automatic parameter update
// request is enabled.
#define DEFAULT_DESIRED_MIN_CONN_INTERVAL 80 // 8

// Maximum connection interval (units of 1.25ms) if automatic parameter update
// request is enabled.
#define DEFAULT_DESIRED_MAX_CONN_INTERVAL 800// 8

// Slave latency to use if automatic parameter update request is enabled
#define DEFAULT_DESIRED_SLAVE_LATENCY 0 // 50

// Supervision timeout value (units of 10ms) if automatic parameter update
// request is enabled.
//超时时间,就是两个设备在连接的这段时间没有发生通讯而导致连接自动断开的值。Range(10ms-----32s)
#define DEFAULT_DESIRED_CONN_TIMEOUT 1000//500

// Whether to enable automatic parameter update request when a connection is
// formed.
#define DEFAULT_ENABLE_UPDATE_REQUEST GAPROLE_LINK_PARAM_UPDATE_INITIATE_BOTH_PARAMS

// Connection Pause Peripheral time value (in seconds)
#define DEFAULT_CONN_PAUSE_PERIPHERAL 5// 10

// Default GAP pairing mode
#define DEFAULT_PAIRING_MODE GAPBOND_PAIRING_MODE_WAIT_FOR_REQ //GAPBOND_PAIRING_MODE_INITIATE //

// Default MITM mode (TRUE to require passcode or OOB when pairing)
#define DEFAULT_MITM_MODE FALSE

// Default bonding mode, TRUE to bond
#define DEFAULT_BONDING_MODE TRUE

// Default GAP bonding I/O capabilities
#define DEFAULT_IO_CAPABILITIES GAPBOND_IO_CAP_NO_INPUT_NO_OUTPUT

// Battery level is critical when it is less than this %
#define DEFAULT_BATT_CRITICAL_LEVEL 6