This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F 使用host_test工程问题

Expert 2290 points

我下载cc2640r2lp_host_test.hex文件到板子, 使用这个板子和BTool对其它设备进行更新,  我想把跳转到OAD更新的指令改变, 但是我在host_test工程没有找到改变的地方.

下面是BTool中显示指令

[20] : <Tx> - 09:48:51.408
-Type : 0x01 (Command)
-OpCode : 0xFD96 (GATT_WriteLongCharValue)
-Data Length : 0x07 (7) byte(s)
ConnHandle : 0x0000 (0)
Handle : 0x0033 (51)
Offset : 0x0000 (0)
Value : 01
Dump(Tx):
0000:01 96 FD 07 00 00 33 00 00 00 01

这个可以改变上面的Value的值吗?

这个实在host_test工程中实现的吗