This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F使用UART同时使用SPI时UART不工作

工程师们你们好,

请问一下,我有一个UART线程来进行UART的读写操作,之后我初始化了一个SPI,增加这个SPI之后,UART的线程无法工作,在CS调试模式下无法标记断点无法进入,但是SPI是可以发送出数据的,在另一块板子上可以收到数据,UART波特率为921600,SPI为1000000,这两个之间会有影响吗?SPI是master模式,这两个同时使用会有问题吗?

  • SPI和串口可以同时使用,不知道你具体是哪里的问题,需要提供一下代码
  • #include <stdint.h>
    #include <stddef.h>
    #include <SPI_Device.h>
    
    #include "ti/drivers/SPI.h"
    #include "ti/drivers/spi/***.h"
    #include "ti/drivers/dma/UDMACC26XX.h"
    
    #include "uartdebug.h"
    
    
    #include "board.h"
    #include "string.h"
    #define SPI_DATA_LEN 20
    
    SPI_Params SPI_DeviceParam;
    SPI_Handle SPI_DeviceHandle;
    SPI_Transaction SPI_DeviceTransAct;
    char SpiRxBuf[SPI_DATA_LEN];
    char SpiTxBuf[SPI_DATA_LEN];
    
    // 中断
    void SPI_DeviceCallback (SPI_Handle handle, SPI_Transaction *transaction)
    {
        UART_Handle uart1 = GetUartHandle();
        // Start another transfer
        SPI_transfer(handle, transaction);
        UART_write(uart1, transaction->rxBuf, 20);
    }
    
    // 初始化
    void SPI_DeviceInit(void)
    {
        SPI_init();
    
        SPI_DeviceTransAct.count = SPI_DATA_LEN;
        SPI_DeviceTransAct.rxBuf = SpiRxBuf;
        SPI_DeviceTransAct.txBuf = SpiTxBuf;
    
        SPI_Params_init(&SPI_DeviceParam);
    
        SPI_DeviceParam.transferMode = SPI_MODE_CALLBACK;
        SPI_DeviceParam.mode = SPI_MASTER;
        SPI_DeviceParam.frameFormat = SPI_POL1_PHA1;
        SPI_DeviceParam.transferCallbackFxn = SPI_DeviceCallback;
        SPI_DeviceParam.bitRate = 1000000;
    
        SPI_DeviceHandle = SPI_open(0, &SPI_DeviceParam);
    
        if ( 0 > SPI_control(SPI_DeviceHandle, ***, NULL) )
        {
            while(1);
        }
    
        SPI_transfer(SPI_DeviceHandle, &SPI_DeviceTransAct);
    }
    
    // 发送
    void SPI_DeviceSendData(void)
    {
        strncpy(SpiTxBuf, "01234567890123456789", SPI_DATA_LEN);
        SPI_transfer(SPI_DeviceHandle, &SPI_DeviceTransAct);
    }

    您好,以上是我的代码,当做主机发送20个字节,片选引脚配置的是IO11,在从机模式下能够工作,UART也是正常的,主机修改过后则UART不工作,

      /* Kick off application - Priority 1 */
      SimpleCentral_createTask();
    
      //Uart init
      UartThread_createTask();
    
      SPI_DeviceInit();

    这是main中初始化部分,麻烦您看下,谢谢!

  • 这是我自己给写死了,搞定了!

    /*!
    * @brief Function to perform SPI transactions
    *
    * If the SPI is in #SPI_MASTER mode, it will immediately start the
    * transaction. If the SPI is in #SPI_SLAVE mode, it prepares the driver for
    * a transaction with a SPI master device. The device will then wait until
    * the master begins the transfer.
    *
    * In #SPI_MODE_BLOCKING, #SPI_transfer() will block task execution until the
    * transaction has completed or a timeout has occurred.
    *
    * In #SPI_MODE_CALLBACK, %SPI_transfer() does not block task execution, but
    * calls a #SPI_CallbackFxn once the transfer has finished. This makes
    * %SPI_tranfer() safe to be used within a Task, software or hardware
    * interrupt context. If queued transactions are supported SPI_Transfer may
    * be called multiple times to queue multiple transactions. If the driver does
    * not support this functionality additional calls will return false. Refer to
    * device specific SPI driver documentation for support information.
    *
    * From calling #SPI_transfer() until transfer completion, the #SPI_Transaction
    * structure must stay persistent and must not be altered by application code.
    * It is also forbidden to modify the content of the #SPI_Transaction.txBuf
    * during a transaction, even though the physical transfer might not have
    * started yet. Doing this can result in data corruption. This is especially
    * important for slave operations where SPI_transfer() might be called a long
    * time before the actual data transfer begins.
    *
    * @param handle A #SPI_Handle
    *
    * @param transaction A pointer to a #SPI_Transaction. All of the fields within
    * transaction except #SPI_Transaction.count and
    * #SPI_Transaction.status are WO (write-only) unless
    * otherwise noted in the driver implementations. If a
    * transaction timeout has occurred, #SPI_Transaction.count
    * will contain the number of frames that were transferred.
    * Neither is it allowed to modify the transaction object nor
    * the content of #SPI_Transaction.txBuf until the transfer
    * has completed.
    *
    * @return @p true if started successfully; else @p false
    *
    * @sa #SPI_open
    * @sa #SPI_transferCancel
    */
    extern bool SPI_transfer(SPI_Handle handle, SPI_Transaction *transaction);