This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F 支持硬件I2C吗

Expert 2290 points

Other Parts Discussed in Thread: CC2640R2F, CC2640

CC2640R2F 支持硬件I2C吗? 如果支持硬件I2C的最大传输速度是多少? 有相关的文档说明吗?

  • 有硬件I2C,传输速率可自己配置,代码里有如下几种:

    typedef enum {
        I2C_100kHz     = 0,    /*!< I2C Standard-mode. Up to 100 kbit/s. */
        I2C_400kHz     = 1,    /*!< I2C Fast-mode. Up to 400 kbit/s. */
        I2C_1000kHz    = 2,    /*!< I2C Fast-mode Plus. Up to 1Mbit/s. */
        I2C_3330kHz    = 3,    /*!< I2C High-speed mode. Up to 3.4Mbit/s. */
        I2C_3400kHz    = 3,    /*!< I2C High-speed mode. Up to 3.4Mbit/s. */
    } I2C_BitRate;

    代码链接:http://dev.ti.com/tirex/explore/node?node=AHLmQux2wAaoYaHFItp0bw__krol.2c__LATEST

  • #define I2C0_SCL0 IOID_12 //i2c SCL
    #define I2C0_SDA0 IOID_13 //i2c SDA

    typedef enum CC2640R2_LAUNCHXL_I2CName {
    CC2640R2_LAUNCHXL_I2C0 = 0,
    CC2640R2_LAUNCHXL_I2CCOUNT
    } CC2640R2_LAUNCHXL_I2CName;

    I2CCC26XX_Object _i2cCC26xxObjects[CC2640R2_LAUNCHXL_I2CCOUNT];

    const I2CCC26XX_HWAttrsV1 _i2cCC26xxHWAttrs[CC2640R2_LAUNCHXL_I2CCOUNT] =
    {
    {
    .baseAddr = I2C0_BASE,
    .powerMngrId = PowerCC26XX_PERIPH_I2C0,
    .intNum = INT_I2C_IRQ,
    .intPriority = ~0,
    .swiPriority = 0,
    .sdaPin = I2C0_SDA0,
    .sclPin = I2C0_SCL0,
    }
    };

    const I2C_Config cc26xxI2C_config[CC2640R2_LAUNCHXL_I2CCOUNT] =
    {
    {
    .fxnTablePtr = &I2CCC26XX_fxnTable,
    .object = &_i2cCC26xxObjects[CC2640R2_LAUNCHXL_I2C0],
    .hwAttrs = &_i2cCC26xxHWAttrs[CC2640R2_LAUNCHXL_I2C0]
    },
    };

    //I2C 句柄及参数
    static I2C_Handle cc2640_I2C_Handle;
    static I2C_Params cc2640_I2C_Params;
    static I2C_Transaction transaction;

    //初始化I2C
    void i2c_init(void)
    {
    I2C_Params_init(&cc2640_I2C_Params);
    cc2640_I2C_Params.transferMode = I2C_MODE_BLOCKING;
    cc2640_I2C_Params.bitRate = I2C_3330kHz;
    cc2640_I2C_Params.transferCallbackFxn = NULL;
    cc26xxI2C_config[CC2640R2_LAUNCHXL_I2C0].fxnTablePtr->initFxn((I2C_Handle)&cc26xxI2C_config[CC2640R2_LAUNCHXL_I2C0]);
    cc2640_I2C_Handle = cc26xxI2C_config[CC2640R2_LAUNCHXL_I2C0].fxnTablePtr->openFxn((I2C_Handle)&cc26xxI2C_config[CC2640R2_LAUNCHXL_I2C0],&cc2640_I2C_Params);
    if (cc2640_I2C_Handle == NULL)
    {
    *((uint32 *)0x40082270) = 1;
    }
    }

    我按上面的程序配置 SCL都是只有300多KHz左右, 上面的配置有问题吗? 还是CC2640R2F硬件I2C有最大频率限制?

  • 手册上原文是这样:The I 2C interface is used to communicate with devices compatible with the I 2C standard. The I 2C interface is capable of 100-kHz and 400-kHz operation, and can serve as both I 2C master and I 2C slave.

    因为实验室里我们只测试并验证了 100-kHz和 400-kHz ,但是有客户设置过其他值,1M以下应该都没有问题。

  • 硬件I2C中的起始和结束时间是多少,
  • I2C起始和结束的时间请查看时序图
  • 硬件I2C只是发送或接收数据而已, 起始和停止不处理?
  • 时序在底层已处理,开放给用户的是直接调用的API接口
  • 有没有时序图提供, 我是使用硬件I2C驱动OLED显示.
  • I2C时序图网上搜一下就有了
  • CC2640R2F I2C的从机地址只有7位, 不包含读写位的吗?