This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F 定时器边缘计数模式

GPTimerCC26XX_Handle hTimer;
void timerCallback(GPTimerCC26XX_Handle handle, GPTimerCC26XX_IntMask interruptMask) {
    // interrupt callback code goes here. Minimize processing in interrupt.
}
void taskFxn(uintptr_t a0, uintptr_t a1) {
  GPTimerCC26XX_Params params;
  GPTimerCC26XX_Params_init(&params);
  params.width          = GPT_CONFIG_16BIT;
  params.mode           = GPT_MODE_PERIODIC;
  params.direction      = GPTimerCC26XX_DIRECTION_UP;
  params.debugStallMode = GPTimerCC26XX_DEBUG_STALL_OFF;
  hTimer = GPTimerCC26XX_open(CC2650_GPTIMER0A, &params);
  if(hTimer == NULL) {
    Log_error0("Failed to open GPTimer");
    Task_exit();
  }
  Types_FreqHz  freq;
  BIOS_getCpuFreq(&freq);
  GPTimerCC26XX_Value loadVal = freq.lo / 1000 - 1; //47999
  GPTimerCC26XX_setLoadValue(hTimer, loadVal);
  GPTimerCC26XX_registerInterrupt(hTimer, timerCallback, GPT_INT_TIMEOUT);
  GPTimerCC26XX_start(hTimer);
  while(1) {
    Task_sleep(BIOS_WAIT_FOREVER);
  }
}

如果我将TIMER的工作模式改成了GPT_MODE_EDGE_COUNT ,并用GPTimerCC26XX_getValue来获取一段时间内我捕获的边缘数目。那在上面的范例代码中,周期计时模式是在定时时间到达后调用回调函数 timerCallback的,但是如果是EDGE_COUNT模式呢?回调函数是在什么时候调用?是在定时时间结束吗?

如果是定时时间结束后调用?我是不是可以在回调函数中使用GPTimerCC26XX_getValue来获取该时间段内捕获的边缘数目?

  • 你说的GPT_MODE_EDGE_COUNT和EDGE_COUNT不是同一个模式吗,是在定时时间结束后调用
  • 是一样的,我在代码实现的时候他一直在等待边缘事件的发生,但我并不知道它到底在检测哪个引脚的事件,比如说我想用DIO21来检测脉冲数量,要怎么配置我的输入端口?
  • GPTimerCC26XX_Handle hTimer;
    GPTimerCC26XX_Value timer_Value;
    static PIN_State TimerPins;
    static PIN_Handle TimerPinHandle = NULL;
    
    PIN_Config TimerinitTable[] = {
        PIN_TIMER | PIN_INPUT_EN | PIN_PULLUP | PIN_IRQ_BOTHEDGES |
        PIN_HYSTERESIS,
        PIN_TERMINATE
    };
    
    
    void timerCallback(GPTimerCC26XX_Handle handle, GPTimerCC26XX_IntMask interruptMask) {
         // interrupt callback code goes here. Minimize processing in interrupt.
        timer_Value = GPTimerCC26XX_getValue(hTimer);
        Log_info0("timer_working!");
        Log_info1("Value is %d",timer_Value);
    
     }
    extern void timer_init(void)
    {
        if(TimerPinHandle==NULL)
        {
            TimerPinHandle = PIN_open(&TimerPins,TimerinitTable);
        }
        PINCC26XX_setMux(TimerPinHandle, PIN_TIMER, GPT_PIN_0A );
        GPTimerCC26XX_Params params;
        GPTimerCC26XX_Params_init(&params);
        params.width          = GPT_CONFIG_16BIT;
        params.mode           = GPT_MODE_EDGE_COUNT;
        params.direction      = GPTimerCC26XX_DIRECTION_UP;
        params.debugStallMode = GPTimerCC26XX_DEBUG_STALL_OFF;
        hTimer = GPTimerCC26XX_open(Board_GPTIMER0A, &params);
        if(hTimer == NULL) {
            Log_error0("Failed to open GPTimer");
            Task_exit();
        }
    
        xdc_runtime_Types_FreqHz  freq;
        BIOS_getCpuFreq(&freq);
        GPTimerCC26XX_Value loadVal = freq.lo / 100 - 1;
        GPTimerCC26XX_setLoadValue(hTimer, loadVal);
        GPTimerCC26XX_registerInterrupt(hTimer, timerCallback, GPT_INT_CAPTURE);
        GPTimerCC26XX_setCaptureEdge(hTimer,GPTimerCC26XX_BOTH_EDGES);
    
        GPTimerCC26XX_start(hTimer);
    
    }

    我按照历程写了边缘捕获的代码,但并没有成功调用回调函数,这是什么环节出现问题呢?

  • 你用的是哪个例程?
  • file:///home/magic/ti/simplelink_cc2640r2_sdk_4_10_00_10/docs/tidrivers/doxygen/html/_g_p_timer_c_c26_x_x_8h.html#ab4a2e82c659e0ea1fa2ae7a852298359a46af9b3278d2116fd4862c7fe19624b7
  • 这部分代码的功能只是利用定时器产生中断,参考下这里:e2e.ti.com/.../433597

  • 设置引脚用PINCC26XX_setMux()

    PIN_Status PINCC26XX_setMux ( PIN_Handle handle,
    PIN_Id pinId,
    int32_t nMux
    )

    Connect pin to HW peripheral, signal or to GPIO.

    Parameters
    handle Handle provided by previous call to PIN_open()
    pinId Pin ID
    nMux Device-specific index of peripheral port or hardware signal. A value of -1 reverts the pin to GPIO mapping
    Returns
    PIN_SUCCESS if successful, else error code
    Note
    Mostly used by driver code or for diagnostics
    Usage
    PIN_setMux(hPins, PIN_ID(16), PINCC26XX_UART_TX);
  • /*!
     *  @brief
     *  Definitions for supported GPTimer interrupts. GPTimerCC26XX_IntMask
     *  arguments should be a bit vector containing these definitions.
     *  See description in Technical Reference
     */
    typedef enum GPTimerCC26XX_Interrupt
    {
        GPT_INT_TIMEOUT           = 1 << 0,
            GPT_INT_CAPTURE_MATCH = 1 << 1,
            GPT_INT_CAPTURE       = 1 << 2,
            GPT_INT_MATCH         = 1 << 3,
    } GPTimerCC26XX_Interrupt;
            GPT_INT_CAPTURE_MATCH = 1 << 1,
            GPT_INT_CAPTURE       = 1 << 2,
            GPT_INT_MATCH         = 1 << 3,

    这三种模式都是如何触发中断的??为什么我选择GPT_INT_CAPTURE就不会触发中断,但使用GPT_INT_CAPTURE_MATCH就可以
    没有看到这三个触发条件的详细描述阿,能解释下吗