This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2640的IO口做输入检测电平问题

做5v输入检测,理论上用电阻32.4K和20K分压出3.3V,IO检测出高电平即可。实际操作不管IO输入设置为上拉、下拉还是浮空都会因为IO本身内阻问题,导致实际分压不准。

提问:

1、这边如果不修改电阻值得情况下,能否通过设置IO将内阻问题规避掉,达到理论效果。

2、改电阻话,设置多大才能避免内阻拉电流。