This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640 低功耗模式怎么实现



目前的系统使用协议栈的例程实现连接手机。通过蓝牙模块io连接,按下后给手机发送vol-,up、down、right、left信息。

使用到

1、定时器,每隔100ms扫描按键情况。

2、ADC检测电压。也是放在定时器中100ms检测一次。

现在想实现低功耗

1、除了将定义POWER_SAVING 代码哪里要改动?目前定义了POWER_SAVING后定时器无法运行

2、当ADC检测到电压低于3.3V后,想要进入休眠模式,当高于3.3V后退出休眠模式。如何实现。