This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教一下,想CC2640R2F例程中SimpleBLEbroadcaster 通过按键控制 shutdown和唤醒,在设置shutdown按键时候,发现第一次按下手机搜不到;但是第二次按下去,又会搜索到simpleBLEbroadcaster,shutdown按键变成了唤醒按键,这是为什么,希望能够得到指导,谢谢



这是按键的部分,按下shutdown按键后,再按一次,设备又可以被手机搜到了
static void GUA_HandleKeys(uint8 GUA_keys)
{
  //按键
  if ( GUA_keys & GUA_KEY_VALUE )
  {
      GUA_Led_Set(HAL_LED_2, HAL_LED_MODE_OFF);
      Power_shutdown(0, 0);
  }

  if ( GUA_keys & GUA_KEY_VALUE_2 )
  {
    GUA_Led_Set(HAL_LED_2, HAL_LED_MODE_ON);        
  }
}

  • 看下这里,是不是将其设为唤醒引脚了

    /** @brief Configure wakeup (from shutdown) on pins
     *
     *  @param aPinCfg #PIN_Config list identifying pin ID and relevant pin
     *                 configuration as one of:
     *                 - #PINCC26XX_NO_WAKEUP      (default)
     *                 - #PINCC26XX_WAKEUP_POSEDGE
     *                 - #PINCC26XX_WAKEUP_NEGEDGE
     *  @return #PIN_SUCCESS if successful, else error code
     *
     *  @par Usage
     *       @code
     *       PIN_setWakeup(NULL, PIN_ID(9)|PIN_WAKEUP_NEGEDGE);
     *       Power_shutdown(0, 0);
     *       @endcode
     *
     *  @note A wake-up event to wake up from shutdown is not detected until
     *  the device reaches shutdown. Wake-up events happening after a shutdown
     *  is initiated but before actual shutdown are not captured and thus will
     *  not cause the device to wake up.
     */
    extern PIN_Status PINCC26XX_setWakeup(const PIN_Config aPinCfg[]);