This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R1

您好:

我在使用CC2652R1时出现死机问题,只要不断进行搜索扫描就会出现死机。使用IAR8.32.3,协议栈版本为:simplelink_cc13x2_26x2_sdk_4_20_00_35,工程为Multi role。

程序参数配置为:

/// Default scan interval (in 625 us ticks)

#define SCAN_PARAM_DFLT_INTERVAL           800

/// Default scan window   (in 625 us ticks)

#define SCAN_PARAM_DFLT_WINDOW             800

  GapScan_setPhyParams(DEFAULT_SCAN_PHY, SCAN_TYPE_ACTIVE,

                       SCAN_PARAM_DFLT_INTERVAL, SCAN_PARAM_DFLT_WINDOW);

// Default scan duration in 10 ms

#define DEFAULT_SCAN_DURATION                   100

然后每10s执行一次:

GapScan_enable(0, DEFAULT_SCAN_DURATION, 0);

就会进入死机状态。

死机时的现象:

请问是什么原因?谢谢。