This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640 示波器电流分析?



如下图所示,上面第一幅图是我测的,设置广播间隔时间1s,为什么每一个1s间隔会出现两个这种波?

下面一副图和TI的蓝牙广播功耗分析里每次间隔只有一个波?

想知道怎么两个波怎么设置出来的,有什么用?怎么关闭来减少功耗?

  • 下面那个电流波形才是正常的,有个recharge,请看一下这里recharge的解释:www.ti.com/.../swra478d.pdf  看错了,那个尖峰应该是唤醒进行广播的功耗
     
    上面那个波形,看着像其他有任务在运行

  • 我好像找到了:e2e.ti.com/.../880139

    TI例程开了 advHandleLongRange 和 advHandleLongRange 两个广播,我广播间隔设置都是1s ,所以一直一起出来,我把advHandleLongRange 关了,大概正常了,只有充电电流和1s钟的广播电流。
    static void SimplePeripheral_processGapMessage(gapEventHdr_t *pMsg)
    {
    switch(pMsg->opcode)
    {
    case GAP_DEVICE_INIT_DONE_EVENT:
    {
    bStatus_t status = FAILURE;

    gapDeviceInitDoneEvent_t *pPkt = (gapDeviceInitDoneEvent_t *)pMsg;

    if(pPkt->hdr.status == SUCCESS)
    {
    // Store the system ID
    uint8_t systemId[DEVINFO_SYSTEM_ID_LEN];

    // use 6 bytes of device address for 8 bytes of system ID value
    systemId[0] = pPkt->devAddr[0];
    systemId[1] = pPkt->devAddr[1];
    systemId[2] = pPkt->devAddr[2];

    // set middle bytes to zero
    systemId[4] = 0x00;
    systemId[3] = 0x00;

    // shift three bytes up
    systemId[7] = pPkt->devAddr[5];
    systemId[6] = pPkt->devAddr[4];
    systemId[5] = pPkt->devAddr[3];

    // Set Device Info Service Parameter
    DevInfo_SetParameter(DEVINFO_SYSTEM_ID, DEVINFO_SYSTEM_ID_LEN, systemId);

    Display_printf(dispHandle, SP_ROW_STATUS_1, 0, "Initialized");

    // Setup and start Advertising
    // For more information, see the GAP section in the User's Guide:
    // software-dl.ti.com/.../

    // Temporary memory for advertising parameters for set #1. These will be copied
    // by the GapAdv module
    GapAdv_params_t advParamLegacy = GAPADV_PARAMS_LEGACY_SCANN_CONN;

    // Create Advertisement set #1 and assign handle
    status = GapAdv_create(&SimplePeripheral_advCallback, &advParamLegacy,
    &advHandleLegacy);
    SIMPLEPERIPHERAL_ASSERT(status == SUCCESS);

    // Load advertising data for set #1 that is statically allocated by the app
    status = GapAdv_loadByHandle(advHandleLegacy, GAP_ADV_DATA_TYPE_ADV,
    sizeof(advertData), advertData);
    SIMPLEPERIPHERAL_ASSERT(status == SUCCESS);

    // Load scan response data for set #1 that is statically allocated by the app
    status = GapAdv_loadByHandle(advHandleLegacy, GAP_ADV_DATA_TYPE_SCAN_RSP,
    sizeof(scanRspData), scanRspData);
    SIMPLEPERIPHERAL_ASSERT(status == SUCCESS);

    // Set event mask for set #1
    status = GapAdv_setEventMask(advHandleLegacy,
    GAP_ADV_EVT_MASK_START_AFTER_ENABLE |
    GAP_ADV_EVT_MASK_END_AFTER_DISABLE |
    GAP_ADV_EVT_MASK_SET_TERMINATED);

    // Enable legacy advertising for set #1
    status = GapAdv_enable(advHandleLegacy, GAP_ADV_ENABLE_OPTIONS_USE_MAX , 0);
    SIMPLEPERIPHERAL_ASSERT(status == SUCCESS);

    // // Use long range params to create long range set #2
    // GapAdv_params_t advParamLongRange = GAPADV_PARAMS_AE_LONG_RANGE_CONN;
    //
    // // Create Advertisement set #2 and assign handle
    // status = GapAdv_create(&SimplePeripheral_advCallback, &advParamLongRange,
    // &advHandleLongRange);
    // SIMPLEPERIPHERAL_ASSERT(status == SUCCESS);
    //
    // // Load advertising data for set #2 that is statically allocated by the app
    // status = GapAdv_loadByHandle(advHandleLongRange, GAP_ADV_DATA_TYPE_ADV,
    // sizeof(advertData), advertData);
    // SIMPLEPERIPHERAL_ASSERT(status == SUCCESS);
    //
    // // Set event mask for set #2
    // status = GapAdv_setEventMask(advHandleLongRange,
    // GAP_ADV_EVT_MASK_START_AFTER_ENABLE |
    // GAP_ADV_EVT_MASK_END_AFTER_DISABLE |
    // GAP_ADV_EVT_MASK_SET_TERMINATED);
    //
    // // Enable long range advertising for set #2
    // status = GapAdv_enable(advHandleLongRange, GAP_ADV_ENABLE_OPTIONS_USE_MAX , 0);
    // SIMPLEPERIPHERAL_ASSERT(status == SUCCESS);

    #ifdef PTM_MODE
    直接这里注释应该没问题把?