使用的是simplelink_cc2640r2_sdk_1_40_00_45版本SDK
从机使用的CC2640R2F的YFV封装
主机使用的是CC2640R2F的RGZ封装
目前手上有两块RGZ的板子,一块是开发板1,一块是自己画的板子2(没有接32.768K的晶振)
板子1可以和从机完成正常的通信过程,包括connect,pair、writeChar、readChar等
板子2可以扫描到从机,但是一直连接失败,会交替出现connected failed reason 49和Disconnected reason 62(是使能的pair的,后面取消pair,还是类似的情况)
因为之前使用CC2640R2FYFV做从机时也是没接32.768K晶振的,遇到类似的情况。当时是在simple_peripheral项目下选择了FlahROM_StackLibrary_RCOSC。现在觉得可能也是这个晶振的问题,想用同样的方法解决发现simple_central的项目下没有RCOSC这个选项
想请问下,主机是否是必须要接32.768K晶振,如果可以不接,软件上应该怎样去做配置?谢谢