hi!我使用的是ble-stack ,我将一些使用的记录储存在一个252字节的缓冲区中,我希望CC2640R2F能够将这252个字节传输到我的手机上,notify可以胜任这个功能吗?一次性传输252个字节,最大的传数量为多少呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用CC2640R2F的话,新版SDK已经默认开启Data Length Extension了,也就是设备连接后会发起数据包大小协商,如果双方都使能了DLE,即可传输251字节。代码可参考simple peripheral/central
// Set default values for Data Length Extension
// Extended Data Length Feature is already enabled by default
{
// Set initial values to maximum, RX is set to max. by default(251 octets, 2120us)
// Some brand smartphone is essentially needing 251/2120, so we set them here.
#define APP_SUGGESTED_PDU_SIZE 251 //default is 27 octets(TX)
#define APP_SUGGESTED_TX_TIME 2120 //default is 328us(TX)
// This API is documented in hci.h
// See the LE Data Length Extension section in the BLE5-Stack User's Guide for information on using this command:
// software-dl.ti.com/.../
HCI_LE_WriteSuggestedDefaultDataLenCmd(APP_SUGGESTED_PDU_SIZE, APP_SUGGESTED_TX_TIME);
}