This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

#cc2640r2f oad oad_image_tool问题

 在按照C:\ti_140\simplelink_cc2640r2_sdk_1_40_00_45\docs\ble5stack\ble_user_guide下的手册移植OAD程序时出现

Error while running C:\ti_140\simplelink_cc2640r2_sdk_1_40_00_45\tools\ble5stack\oad\
oad_image_tool.exe C:\ti_140\simplelink_cc2640r2_sdk_1_40_00_45\examples\rtos\
CC2640R2_LAUNCHXL\ble5stack\simple_peripheral\tirtos\iar\app\FlashROM_StackLibrary\Exe\
ble5_simple_peripheral_cc2640r2lp_app_FlashROM_StackLibrary.hex -t offchip -i app --imgVer 0 -ob 
C:\ti_140\simplelink_cc2640r2_sdk_1_40_00_45\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\
simple_peripheral\tirtos\iar\app\FlashROM_StackLibrary\Exe\1.bin -m 0x0000 --r 0x0000

上面我将路径改为绝对路径了,还是报错

使用WINDOW下cmd运行:

Version: 1.0
******************************************************************************************
OAD Type: offchip
Img Type: APP
Input file(s): ble5_simple_peripheral_cc2640r2lp_app_FlashROM_StackLibrary.hex
Output Hex file: None
Output Bin file: 1.bin
Layout of concatenated input files, per flash sector, before applying --range.
 00 | 01 | 02 | 03 | 04 | 05 | 06 | 07 | 08 | 09 | 10 | 11 | 12 | 13 | 14 | 15
XX0X XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX
XX00 XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX
XX00 XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX
XXX0 XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX
 16 | 17 | 18 | 19 | 20 | 21 | 22 | 23 | 24 | 25 | 26 | 27 | 28 | 29 | 30 | 31
XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX 0000 0000 0000 0000 0000 000X 000x ----
XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX X000 0000 0000 0000 0000 0000 0000 ----
XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX X000 0000 0000 0000 0000 0000 0000 ----
XXXX XXXX XXXX XXXX XXXX XXXX XXXX XXXX X000 0000 0000 0000 0000 0000 0000 ----
  Legend: `X` 100% full, `x` >50% full, `.` <50% full, `-` empty, `F` all 0xFF,
  `0` all 0x00.
******************************************************************************************
Runtime Output:
Fatal Error: -- The provided metadata location (0x00000000) is not empty. Exiting.
我APP是可以下载到程序中正常运行的