This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SDK3.4中AOA功能切换天线组



您好,我有一个关于AOA功能天线组切换的问题想咨询下。

目前我在做AOA功能的测试

SDK版本是3.40,我使用rtls_aoa_iq_with_rtls_util_export_into_csv_save.py获取IQ数据,

"aoa_cc26x2": {
"aoa_slot_durations": 1,
"aoa_sample_rate": 1,
"aoa_sample_size": 1,
"aoa_sampling_control": int('0x10', 16),
## bit 0 - 0x00 - default filtering, 0x01 - RAW_RF no filtering,
## bit 4,5 - default: 0x10 - ONLY_ANT_1, optional: 0x20 - ONLY_ANT_2
"aoa_sampling_enable": 1,
"aoa_pattern_len": 3,
"aoa_ant_pattern": [0, 1, 2]
}

"aoa_sampling_control": int('0x10', 16),使用的是天线组1,功能正常

现在我想使能天线组2,aoa_sampling_control 设置为:"aoa_sampling_control": int('0x20', 16),

但是我收到的IQ数据好像还是天线组1的,因为计算出来的角度没有变

请问我启用天线组2的方法正确吗,如果我想同时启用两组天线可以实现吗,如何设置?

  • 无法同时使用两个阵列天线,只能进行切换。方法是修改修改python脚本中的"aoa_sampling_control"

    _sampling_control的有效值只有: 0x10, 0x20, 0x11 and 0x21.
    Bit 0 selects the filtering type => 0x00 for default filtering, 0x01 for RAW_RF / no filtering.
    Bit 4 and 5 selects the antenna array to use => 0x10 for ONLY_ANT_1, 0x20 for ONLY_ANT_2
  • 感谢你的及时回复, 我知道是通过aoa_sampling_control设置切换阵列天线,我现在碰到的问题是:切换了阵列天线感觉没有切换成功,因为我切换两组天线阵列 获取的IQ计算的相位差,AOA角度没有明显变化,

    我在SDK代码中有看到这样一段代码:

    void AOA_init(uint8_t startAntenna)
    {
    #ifdef RTLS_PASSIVE
    uint8_t antArray[BOOSTXL_AOA_NUM_ANT + 1] = {ANT2, ANT1, ANT3, ANT_ARRAY};

    // Init only once
    if (gPinHandle == NULL)
    {
    AOA_initAntArray(antArray, BOOSTXL_AOA_NUM_ANT + 1);
    }

    // Initialize ant array switch pin
    if (startAntenna == 2)
    {
    // Start with A2 (ANT_ARRAY pin high is A1, low is A2)
    PINCC26XX_setOutputValue(ANT_ARRAY, 0);
    }
    else
    {
    // Start with A1 (ANT_ARRAY pin high is A1, low is A2)
    PINCC26XX_setOutputValue(ANT_ARRAY, 1);
    }
    #endif
    }

    好像只有PASSIVE的模式才会去设置ANT_ARRAY引脚去切换阵列天线,我现在是MASTER+SLAVE的方式测试,不知道MASTER+SLAVE的方式是否也支持切换阵列天线
  • 切换天线除了修改上述代码以外,还需要注意引脚及相应的代码实现,具体请看这边的讨论:
    e2e.ti.com/.../879770

    其中提到的truth table链接是这个:dev.ti.com/.../node