Other Parts Discussed in Thread: CC2640R2F
Dear Aill
请教一下CC2640R2F SPI的速率可以调整吗?目前只看到配置的数据是2e6 2MHZ的配置
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC2640R2F
Dear Aill
请教一下CC2640R2F SPI的速率可以调整吗?目前只看到配置的数据是2e6 2MHZ的配置
/*! @brief SPI bit rate in Hz
*
* Maximum bit rates supported by hardware:
* Device Family | Slave Max (MHz) | Master Max (MHz) |
* ------------- | ------------------ | ---------------- |
* MSP432P4 | 16 MHz | 24 MHz |
* MSP432E4 | 10 MHz | 60 MHz |
* CC13XX/CC26XX | 4 MHz | 12 MHz |
* CC32XX | 20 MHz | 20 MHz |
*
* Please note that depending on the specific use case, the driver may not
* support the hardware's maximum bit rate.
*/
uint32_t bitRate;
可以的,修改 bitRate