This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-AoA如何同时使用两个天线阵列?

您好!

    我目前正在使用2个BOOSTXL-AoA(passive)+1个slave+1个master进行三角定位,开发板型号为CC26x2R1,使用的sdk版本为最新的4.30.00.54,UI版本为RTLS UI 1.1.0,我发现当两个passive都连接上时,UI可以显示两个BOOSTXL-AoA的测量角度,但都是默认同时使用相同的天线阵列(阵列1或阵列2),现因定位需求,需要一个BOOSTXL-AoA使用天线阵列1进行测量,另一个BOOSTXL-AoA使用天线阵列2进行测量,当在configuration中设置同时使用两个天线阵列时,UI运行出现错误,请问是否能够实现同时使用两个天线阵列?或者对每个BOOSTXL-AoA参数进行单独设置,即一个使用阵列1,另一个使用阵列2?谢谢!