您好!
我想知道RTLS UI 1.1.0中采集的不同信道下的RSS值所代表的意义,是否能通过这些RSS值来粗略获得发射器(psssive)与接受器(slave)之间的距离,如果可以,我该使用哪个信道下的RSS值?我发现示例中可以采集多个信道下的RSS值,是否这些RSS值都代表发射器与接收器之间的RSS值?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
我想知道RTLS UI 1.1.0中采集的不同信道下的RSS值所代表的意义,是否能通过这些RSS值来粗略获得发射器(psssive)与接受器(slave)之间的距离,如果可以,我该使用哪个信道下的RSS值?我发现示例中可以采集多个信道下的RSS值,是否这些RSS值都代表发射器与接收器之间的RSS值?谢谢!
好的谢谢,但您误解我的意思了,关于角度值如何获取我是清楚的,我的问题是基于RSSI的定位,也就是利用RSSI值来估算距离,然后进行三边定位,http://dev.ti.com/tirex/explore/content/simplelink_cc13x2_26x2_sdk_4_30_00_54/docs/ble5stack/ble_user_guide/html/ble-stack-5.x-guide/localization-index-cc13x2_26x2.html这里有关于这部分的介绍,但不是很详细,我想知道文中所提的可用于估算距离的RSSI值是否就是示例中观察到的不同信道下的RSSI值?如果是,应该对这些不同信道下的RSSI值做如何处理(因为估算passive与salve之间的距离需要一个稳定不变的RSSI值)?如果这些信道下的RSSI值不能直接用于估算距离,那么如何获取真正能够用于估算距离的RSSI值?谢谢!