CC2640RSM做的BLE外设使用过程中,偶尔有一些产品在使用过程中突然BLE连接中断,然后测量发现是24M晶振停振了。我们硬件使用24MHz晶振,省略了32768,低频时钟设置成从高频晶振(24M)而不是内部RC获取的,软件方面关闭了省电模式,我的理解是24M晶振震荡会一直工作,不应该停止,毕竟不用省电了,正常工作时用示波器测量确实也一直工作。同时我们程序里打开了看门狗,但一旦出现问题,晶振停振后,看门狗不能让系统复位,只能断电或把复位脚拉低复位,系统才能重新启动。考虑是不是晶振有问题,但出问题后硬件一复位又能正常工作,重新起振。怀疑静电问题,然后我们外接IO口加了TVS突波吸收器,还是存在该现象。软件方面看门狗打开后如果程序跑飞理应给系统复位,而不是关停晶振吧?并且我们关闭了powerSaving省电模式,底层又没有让系统休眠,不是什么地方会导致进入晶振停振状态。麻烦TI技术人员帮忙分析解决,在线等!