This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC26X2与BOOSTXL-AOA使用问题



对于将CC26X2与BOOSTXL-AOA外接天线一起使用时,我测得的角度信息幅度变化很小(45-52°之间)无论我如何摆放其passive和slave的相对位置。且在修改天线2后,无法运行测得角度信息,所以我估计是我的外接天线板没有工作。

我不知道是我外接天线板BOOSTXL-AOA连接方式不对,还是这个例程存在的bug。(SDK3.4和4.1均是)

对于连接方式里面:将开发板上的C51电容切换至外置天线连接点。这个C51电容如何切换。还是不需要切换只需要将JSC连接口连接起来再将引脚对齐即可。我不太确定我的连接方式对不对, 所以我想问下工作人员具体什么情况。