This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问CC2640R2使用SPI通信时,如何设置MOSI的电平幅值?

Other Parts Discussed in Thread: CC2640, ADS1299

这两张示波器的图片,第一幅是CC2640的输出结果,第二幅是其他单片机的输出结果。粉色(3)号通道是MOSI线,CC2640输出的只有2v左右。但是其他单片机是3.3v

目前使用CC2640的SPI读取从设备的ID没有反应,怀疑是这个电平幅值不够的原因。

但是1号通道也就是CS线,CC2640是可以输出到3.3V的。

我尝试了普通的方法来设置MOSI线的幅值,我通过PIN_open函数单独设置MOSI引脚的输出电平的话,SPI就启动不了了,SPI_open函数返回NULL。

SDK版本为1.40.00.45