This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

蓝牙例程multirole该如何理解呢,是否multirole表示这个板子可以同时进行收到数据和发送数据两个功能

Other Parts Discussed in Thread: CC2640R2F

蓝牙例程multirole该如何理解呢,是否multirole表示这个板子可以同时进行收到数据和发送数据两个功能

  • multirole是指主从一体,既可以做主机,又可以做从机
  • 请看此例程的简介【CC2640R2F】:This project demonstrates the capabilities of the Texas Instruments BLE stack to function in multiple simultaneous connection roles. Specifically, the project is capable of functioning as a master and a slave simultaneously, in any combination, while maintaining up to 8 connections. The project is capable of connecting to any central/peripheral device. Any type of legacy pairing/bonding is possible. Parameter updates are supported. Connections can be established in any role. The project supports multiple simultaneous GATT discoveries and/or pairings/bondings.