This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F使用notify方式进行快速数据更新时遇到的问题

Other Parts Discussed in Thread: CC2640R2F

主从都是CC2640R2F,连接参数为8, 8 ,0, 15,使能了pair,失能了bonding

从机使用notify的方式将数据发送给主机,设置事件触发间隔为10ms时,在主机端可以得到一个比较稳定的接收波形(在主机端触发notify事件时,会去翻转一个IO的状态 ,可得到一个波形),翻转间隔在10ms左右,然后大概间隔1s会有一个20ms的翻转间隔,然后在持续时间接近1个小时的时候,ble的连接会断开,并且再也不能成功建立连接,此时主机是可以扫描到从机并且建立连接,只是一直提示连接失败,最后复位主机是不能解决这个问题的,复位从机可以解决,想请问一下这是什么情况?

测试这个是因为我们想获得更快的数据更新速率,之前相同的连接参数下,使用主机readchar的方式可以实现数据更新时间间隔为20ms,上述方法也可以加快到10ms的更新间隔,但是也遇到了上面描述的问题