This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

antenna angle



测试环境:一块连接BOOSTXL-AOA的CC26X2R板卡作MATSER,一块CC26X2R板卡作SLAVE

测试方法:

Task 1 – Running the AoA application

我参照文档里的Task1,使用阵列1的A1.1 A1.2 A1.3,得到了一个确定的角度,比如90°或者60°

再在角度不变的相同环境下使用

Task 4 – Export raw IQ samples to CSV file

导出IQ数据,发现相位变化基本没有。

然后我又使用Task1,但是将天线阵列设置为仅使用A1.1 A1.2,发现角度一直在波动,且波动范围超过40°,这又是为什么呢。