This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642 IO输出32.768K晶振情况

CC2642  是否有可调用的接口可有IO输出外部32.768K晶振的起振情况

  • 可以把32k晶振的信号输出到引脚,请参考TRM 13.3.4节:www.ti.com/.../swcu185d.pdf

    13.3.4 Map the 32-kHz System Clock (LF Clock) to DIO

    The AON IOC contains the output enable control for the 32-kHz LF system clock output, and the clock signal has its own PORTID called AON_CLK32K (0x7). This makes it easy to output the clock signal to a pin. Map the clock to a chosen DIO, and enable the clock output by setting the
    AON_IOC:CLK32KCTL.OE_N register field to 0x0. The following two driver library calls achieve the same result:
    !~#include <driverlib/aon_ioc.h>
    IOCPortConfigureSet(IOIDn, IOC_PORT_AON_CLK32K, IOC_STD_OUTPUT);
    AONIOC32kHzOutputEnable();