Other Parts Discussed in Thread: CC1352R
CC1352R1F3 SimpleLink_CC13x2_CC26x2 SDK_4.30.00.54 导入CC1352R LanchPad --->Ble5_Stack --->simple_broadcaster例程 开启广播结束事件GAP_ADV_EVT_MASK_END,大概运行20分钟左右会造成内存耗尽的问题,表现在广播回调函数种消息入队分配不到内存。 请问这是什么原因造成的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC1352R
CC1352R1F3 SimpleLink_CC13x2_CC26x2 SDK_4.30.00.54 导入CC1352R LanchPad --->Ble5_Stack --->simple_broadcaster例程 开启广播结束事件GAP_ADV_EVT_MASK_END,大概运行20分钟左右会造成内存耗尽的问题,表现在广播回调函数种消息入队分配不到内存。 请问这是什么原因造成的?
你好, 修改如下:
1、 增加事件,simple_broadcaster.c中修改setEventMask函数参数增加GAP_ADV_EVT_MASK_END事件:
// Set event mask
status = GapAdv_setEventMask(advHandleLegacy,
GAP_ADV_EVT_MASK_START_AFTER_ENABLE | GAP_ADV_EVT_MASK_END |
GAP_ADV_EVT_MASK_END_AFTER_DISABLE |
GAP_ADV_EVT_MASK_SET_TERMINATED);
2、SimpleBroadcaster_processAdvEvent函数修改如下:
static bool SimpleBroadcaster_processAdvEvent(sbGapAdvEventData_t *pEventData)
{
bool safeToDealloc = TRUE;
static volatile uint8_t test;
switch (pEventData->event)
{
case GAP_EVT_ADV_START_AFTER_ENABLE:
Display_printf(dispHandle, 2, 0, "Advertising");
break;
case GAP_EVT_INSUFFICIENT_MEMORY:
safeToDealloc = FALSE;
break;
case GAP_EVT_ADV_END:
test++;
break;
default:
// Do nothing.
break;
}
return(safeToDealloc);
}
附上完整simple_broadcaster.文件:
/******************************************************************************
@file simple_broadcaster.c
@brief This file contains the Simple Broadcaster sample application for
use with the CC2650 Bluetooth Low Energy Protocol Stack.
Group: WCS, BTS
Target Device: cc13x2_26x2
******************************************************************************
Copyright (c) 2011-2020, Texas Instruments Incorporated
All rights reserved.
Redistribution and use in source and binary forms, with or without
modification, are permitted provided that the following conditions
are met:
* Redistributions of source code must retain the above copyright
notice, this list of conditions and the following disclaimer.
* Redistributions in binary form must reproduce the above copyright
notice, this list of conditions and the following disclaimer in the
documentation and/or other materials provided with the distribution.
* Neither the name of Texas Instruments Incorporated nor the names of
its contributors may be used to endorse or promote products derived
from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
******************************************************************************
*****************************************************************************/
/*********************************************************************
* INCLUDES
*/
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/knl/Event.h>
#include <ti/sysbios/knl/Queue.h>
#include <ti/display/Display.h>
#include "util.h"
#include <icall.h>
/* This Header file contains all BLE API and icall structure definition */
#include <icall_ble_api.h>
#include <devinfoservice.h>
#ifdef USE_RCOSC
#include "rcosc_calibration.h"
#endif //USE_RCOSC
#include <ti_drivers_config.h>
#include "ti_ble_config.h"
#include "simple_broadcaster.h"
/*********************************************************************
* MACROS
*/
/*********************************************************************
* CONSTANTS
*/
// Task configuration
#define SB_TASK_PRIORITY 1
#ifndef SB_TASK_STACK_SIZE
#define SB_TASK_STACK_SIZE 1024
#endif
#define SB_ADV_EVT 1
// Internal Events for RTOS application
#define SB_ICALL_EVT ICALL_MSG_EVENT_ID // Event_Id_31
#define SB_QUEUE_EVT UTIL_QUEUE_EVENT_ID // Event_Id_30
#define SB_ALL_EVENTS (SB_ICALL_EVT | \
SB_QUEUE_EVT)
// Spin if the expression is not true
#define SIMPLEBROADCASTER_ASSERT(expr) if (!(expr)) HAL_ASSERT_SPINLOCK;
/*********************************************************************
* TYPEDEFS
*/
// App event passed from stack modules. This type is defined by the application
// since it can queue events to itself however it wants.
typedef struct
{
uint8_t event; // event type
void *pData; // pointer to message
} sbEvt_t;
/*********************************************************************
* GLOBAL VARIABLES
*/
// Display Interface
Display_Handle dispHandle = NULL;
/*********************************************************************
* EXTERNAL VARIABLES
*/
/*********************************************************************
* EXTERNAL FUNCTIONS
*/
/*********************************************************************
* LOCAL VARIABLES
*/
// Entity ID globally used to check for source and/or destination of messages
static ICall_EntityID selfEntity;
// Event globally used to post local events and pend on system and
// local events.
static ICall_SyncHandle syncEvent;
// Queue object used for app messages
static Queue_Struct appMsgQueue;
static Queue_Handle appMsgQueueHandle;
// Task configuration
Task_Struct sbTask;
#if defined __TI_COMPILER_VERSION__
#pragma DATA_ALIGN(sbTaskStack, 8)
#else
#pragma data_alignment=8
#endif
uint8_t sbTaskStack[SB_TASK_STACK_SIZE];
// Container to store advertising event data when passing from advertising
// callback to app event. See the respective event in GapAdvScan_Event_IDs
// in gap_advertiser.h for the type that pBuf should be cast to.
typedef struct
{
uint32_t event;
void *pBuf;
} sbGapAdvEventData_t;
// Advertising handles
static uint8 advHandleLegacy;
// Address mode
static GAP_Addr_Modes_t addrMode = DEFAULT_ADDRESS_MODE;
/*********************************************************************
* LOCAL FUNCTIONS
*/
static void SimpleBroadcaster_init(void);
static void SimpleBroadcaster_taskFxn(UArg a0, UArg a1);
static void SimpleBroadcaster_processStackMsg(ICall_Hdr *pMsg);
static void SimpleBroadcaster_processGapMessage(gapEventHdr_t *pMsg);
static void SimpleBroadcaster_processAppMsg(sbEvt_t *pMsg);
static void SimpleBroadcaster_advCallback(uint32_t event, void *pBuf, uintptr_t arg);
static bool SimpleBroadcaster_processAdvEvent(sbGapAdvEventData_t *pEventData);
static status_t SimpleBroadcaster_enqueueMsg(uint8_t event, void *pData);
/*********************************************************************
* PROFILE CALLBACKS
*/
// GAP Role Callbacks
/*
static gapRolesCBs_t simpleBroadcaster_BroadcasterCBs =
{
SimpleBroadcaster_stateChangeCB // Profile State Change Callbacks
};
*/
/*********************************************************************
* PUBLIC FUNCTIONS
*/
/*********************************************************************
* @fn SimpleBroadcaster_createTask
*
* @brief Task creation function for the Simple Broadcaster.
*
* @param none
*
* @return none
*/
void SimpleBroadcaster_createTask(void)
{
Task_Params taskParams;
// Configure task
Task_Params_init(&taskParams);
taskParams.stack = sbTaskStack;
taskParams.stackSize = SB_TASK_STACK_SIZE;
taskParams.priority = SB_TASK_PRIORITY;
Task_construct(&sbTask, SimpleBroadcaster_taskFxn, &taskParams, NULL);
}
/*********************************************************************
* @fn SimpleBroadcaster_init
*
* @brief Initialization function for the Simple Broadcaster App
* Task. This is called during initialization and should contain
* any application specific initialization (ie. hardware
* initialization/setup, table initialization, power up
* notification ...).
*
* @param none
*
* @return none
*/
static void SimpleBroadcaster_init(void)
{
// ******************************************************************
// N0 STACK API CALLS CAN OCCUR BEFORE THIS CALL TO ICall_registerApp
// ******************************************************************
// Register the current thread as an ICall dispatcher application
// so that the application can send and receive messages.
ICall_registerApp(&selfEntity, &syncEvent);
#ifdef USE_RCOSC
// Set device's Sleep Clock Accuracy
#if ( HOST_CONFIG & ( CENTRAL_CFG | PERIPHERAL_CFG ) )
HCI_EXT_SetSCACmd(500);
#endif // (CENTRAL_CFG | PERIPHERAL_CFG)
RCOSC_enableCalibration();
#endif // USE_RCOSC
// Create an RTOS queue for message from profile to be sent to app.
appMsgQueueHandle = Util_constructQueue(&appMsgQueue);
// Open LCD
dispHandle = Display_open(Display_Type_ANY, NULL);
// Register with GAP for HCI/Host messages. This is needed to receive HCI
// events. For more information, see the HCI section in the User's Guide:
// http://software-dl.ti.com/lprf/ble5stack-latest/
GAP_RegisterForMsgs(selfEntity);
//Initialize GAP layer for Peripheral role and register to receive GAP events
GAP_DeviceInit(GAP_PROFILE_BROADCASTER, selfEntity, addrMode, &pRandomAddress);
Display_printf(dispHandle, 0, 0, "BLE Broadcaster");
}
/*********************************************************************
* @fn SimpleBroadcaster_processEvent
*
* @brief Application task entry point for the Simple Broadcaster.
*
* @param none
*
* @return none
*/
static void SimpleBroadcaster_taskFxn(UArg a0, UArg a1)
{
// Initialize application
SimpleBroadcaster_init();
// Application main loop
for (;;)
{
// Get the ticks since startup
uint32_t tickStart = Clock_getTicks();
uint32_t events;
events = Event_pend(syncEvent, Event_Id_NONE, SB_ALL_EVENTS,
ICALL_TIMEOUT_FOREVER);
if (events)
{
ICall_EntityID dest;
ICall_ServiceEnum src;
ICall_HciExtEvt *pMsg = NULL;
if (ICall_fetchServiceMsg(&src, &dest,
(void **)&pMsg) == ICALL_ERRNO_SUCCESS)
{
if ((src == ICALL_SERVICE_CLASS_BLE) && (dest == selfEntity))
{
// Process inter-task message
SimpleBroadcaster_processStackMsg((ICall_Hdr *)pMsg);
}
if (pMsg)
{
ICall_freeMsg(pMsg);
}
}
// If RTOS queue is not empty, process app message.
if (events & SB_QUEUE_EVT)
{
while (!Queue_empty(appMsgQueueHandle))
{
sbEvt_t *pMsg = (sbEvt_t *)Util_dequeueMsg(appMsgQueueHandle);
if (pMsg)
{
// Process message.
SimpleBroadcaster_processAppMsg(pMsg);
// Free the space from the message.
ICall_free(pMsg);
}
}
}
}
}
}
/*********************************************************************
* @fn SimpleBroadcaster_processStackMsg
*
* @brief Process an incoming stack message.
*
* @param pMsg - message to process
*
* @return none
*/
static void SimpleBroadcaster_processStackMsg(ICall_Hdr *pMsg)
{
switch (pMsg->event)
{
case GAP_MSG_EVENT:
SimpleBroadcaster_processGapMessage((gapEventHdr_t*) pMsg);
break;
default:
// do nothing
break;
}
}
/*********************************************************************
* @fn SimpleBroadcaster_processGapMessage
*
* @brief Process an incoming GAP event.
*
* @param pMsg - message to process
*/
static void SimpleBroadcaster_processGapMessage(gapEventHdr_t *pMsg)
{
switch(pMsg->opcode)
{
case GAP_DEVICE_INIT_DONE_EVENT:
{
bStatus_t status = FAILURE;
gapDeviceInitDoneEvent_t *pPkt = (gapDeviceInitDoneEvent_t *)pMsg;
if(pPkt->hdr.status == SUCCESS)
{
// Store the system ID
uint8_t systemId[DEVINFO_SYSTEM_ID_LEN];
// use 6 bytes of device address for 8 bytes of system ID value
systemId[0] = pPkt->devAddr[0];
systemId[1] = pPkt->devAddr[1];
systemId[2] = pPkt->devAddr[2];
// set middle bytes to zero
systemId[4] = 0x00;
systemId[3] = 0x00;
// shift three bytes up
systemId[7] = pPkt->devAddr[5];
systemId[6] = pPkt->devAddr[4];
systemId[5] = pPkt->devAddr[3];
// Set Device Info Service Parameter
DevInfo_SetParameter(DEVINFO_SYSTEM_ID, DEVINFO_SYSTEM_ID_LEN, systemId);
// Display device address
Display_printf(dispHandle, 1, 0, "%s Addr: %s",
(addrMode <= ADDRMODE_RANDOM) ? "Dev" : "ID",
Util_convertBdAddr2Str(pPkt->devAddr));
Display_printf(dispHandle, 2, 0, "Initialized");
if (addrMode > ADDRMODE_RANDOM)
{
// Display the RPA.
Display_printf(dispHandle, 3, 0, "RP Addr: %s",
Util_convertBdAddr2Str(GAP_GetDevAddress(FALSE)));
}
// Setup and start Advertising
// For more information, see the GAP section in the User's Guide:
// http://software-dl.ti.com/lprf/ble5stack-latest/
#ifndef BEACON_FEATURE
advParams1.eventProps = GAP_ADV_PROP_SCANNABLE | GAP_ADV_PROP_LEGACY;
#else
advParams1.eventProps = GAP_ADV_PROP_LEGACY;
#endif // !BEACON_FEATURE
// Create Advertisement set
status = GapAdv_create(&SimpleBroadcaster_advCallback, &advParams1,
&advHandleLegacy);
SIMPLEBROADCASTER_ASSERT(status == SUCCESS);
// Load advertising data
status = GapAdv_loadByHandle(advHandleLegacy, GAP_ADV_DATA_TYPE_ADV,
sizeof(advData1), advData1);
SIMPLEBROADCASTER_ASSERT(status == SUCCESS);
// Load scan response data
status = GapAdv_loadByHandle(advHandleLegacy, GAP_ADV_DATA_TYPE_SCAN_RSP,
sizeof(scanResData1), scanResData1);
SIMPLEBROADCASTER_ASSERT(status == SUCCESS);
// Set event mask
status = GapAdv_setEventMask(advHandleLegacy,
GAP_ADV_EVT_MASK_START_AFTER_ENABLE | GAP_ADV_EVT_MASK_END|
GAP_ADV_EVT_MASK_END_AFTER_DISABLE |
GAP_ADV_EVT_MASK_SET_TERMINATED);
SIMPLEBROADCASTER_ASSERT(status == SUCCESS);
// Enable legacy advertising
status = GapAdv_enable(advHandleLegacy, GAP_ADV_ENABLE_OPTIONS_USE_MAX , 0);
SIMPLEBROADCASTER_ASSERT(status == SUCCESS);
}
break;
}
default:
Display_clearLine(dispHandle, 2);
break;
}
}
/*********************************************************************
* @fn SimpleBroadcaster_enqueueMsg
*
* @brief Creates a message and puts the message in RTOS queue.
*
* @param event - message event.
* @param state - message state.
*/
static status_t SimpleBroadcaster_enqueueMsg(uint8_t event, void *pData)
{
uint8_t success;
sbEvt_t *pMsg = ICall_malloc(sizeof(sbEvt_t));
// Create dynamic pointer to message.
if(pMsg)
{
pMsg->event = event;
pMsg->pData = pData;
// Enqueue the message.
success = Util_enqueueMsg(appMsgQueueHandle, syncEvent, (uint8_t *)pMsg);
return (success) ? SUCCESS : FAILURE;
}
return(bleMemAllocError);
}
/*********************************************************************
* @fn SimpleBroadcaster_advCallback
*
* @brief GapAdv module callback
*
* @param pMsg - message to process
*/
static void SimpleBroadcaster_advCallback(uint32_t event, void *pBuf, uintptr_t arg)
{
sbGapAdvEventData_t *pData = ICall_malloc(sizeof(sbGapAdvEventData_t));
if (pData)
{
pData->event = event;
pData->pBuf = pBuf;
if(SimpleBroadcaster_enqueueMsg(SB_ADV_EVT, pData) != SUCCESS)
{
ICall_free(pData);
}
}
}
/*********************************************************************
* @fn SimpleBroadcaster_processAppMsg
*
* @brief Process an incoming callback from a profile.
*
* @param pMsg - message to process
*
* @return None.
*/
static void SimpleBroadcaster_processAppMsg(sbEvt_t *pMsg)
{
bool safeToDealloc = TRUE;
switch (pMsg->event)
{
case SB_ADV_EVT:
safeToDealloc = SimpleBroadcaster_processAdvEvent((sbGapAdvEventData_t*)(pMsg->pData));
break;
default:
// Do nothing.
break;
}
if (safeToDealloc)
{
// Free message data
if (pMsg->pData)
{
ICall_free(pMsg->pData);
}
}
}
/*********************************************************************
* @fn SimpleBroadcaster_processAdvEvent
*
* @brief Process advertising event in app context
*
* @param pEventData
*/
static bool SimpleBroadcaster_processAdvEvent(sbGapAdvEventData_t *pEventData)
{
bool safeToDealloc = TRUE;
static volatile uint8_t test;
switch (pEventData->event)
{
case GAP_EVT_ADV_START_AFTER_ENABLE:
Display_printf(dispHandle, 2, 0, "Advertising");
break;
case GAP_EVT_INSUFFICIENT_MEMORY:
safeToDealloc = FALSE;
break;
case GAP_EVT_ADV_END:
test++;
break;
default:
// Do nothing.
break;
}
return(safeToDealloc);
}
/*********************************************************************
*********************************************************************/
已经定位到问题,这是由于pEventData的内存没有释放导致的,请按照如下代码修改:
static bool SimpleBroadcaster_processAdvEvent(sbGapAdvEventData_t *pEventData)
{
bool safeToDealloc = TRUE;
static volatile uint8_t test;
switch (pEventData->event)
{
case GAP_EVT_ADV_START_AFTER_ENABLE:
Display_printf(dispHandle, 2, 0, "Advertising");
break;
case GAP_EVT_INSUFFICIENT_MEMORY:
safeToDealloc = FALSE;
break;
case GAP_EVT_ADV_END:
test++;
ICall_free(pEventData->pBuf); // fixed memory leak
break;
default:
// Do nothing.
break;
}
return(safeToDealloc);
}
我这边测试发现,使用有限广播方式,一次广播开启6次广播事件,即GapAdv_enable(advHandleLegacy, GAP_ADV_ENABLE_OPTIONS_USE_MAX_EVENTS , 6),保留原始回调事件设置,即
GapAdv_setEventMask(advHandleLegacy,
GAP_ADV_EVT_MASK_START_AFTER_ENABLE |
GAP_ADV_EVT_MASK_END_AFTER_DISABLE |
GAP_ADV_EVT_MASK_SET_TERMINATED);
也同样的会有内存泄漏的问题,每次回调少8个字节,请问是否也采用同样的方法来处理?