This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2640r2f rsm外部中断不能唤醒

由TI 标准例程\simplelink_cc2640r2_sdk_2_20_00_49\examples\rtos\CC2640R2_LAUNCHXL\ble5stack\simple_peripheral修改而来。

删除了CC2640R2_LAUNCHXL,增加了CC2640R2DK_4XS,Display_DISABLE_ALL。按键驱动程序改为如下:

#define Board_BTN1 CC2640R2DK_4XS_KEY_UP
#define Board_BTN2 CC2640R2DK_4XS_KEY_DOWN

/*********************************************************************
* LOCAL FUNCTIONS
*/
static void Board_keyChangeHandler(UArg a0);
static void Board_keyCallback(PIN_Handle hPin, PIN_Id pinId);

/*******************************************************************************
* EXTERNAL VARIABLES
*/

/*********************************************************************
* LOCAL VARIABLES
*/

// Value of keys Pressed
static uint8_t keysPressed;

// Key debounce clock
static Clock_Struct keyChangeClock;

// Pointer to application callback
keysPressedCB_t appKeyChangeHandler = NULL;

// Memory for the GPIO module to construct a Hwi
Hwi_Struct callbackHwiKeys;

// PIN configuration structure to set all KEY pins as inputs with pullups enabled
PIN_Config keyPinsCfg[] =
{

Board_BTN1 | PIN_GPIO_OUTPUT_DIS | PIN_INPUT_EN | PIN_PULLUP,
Board_BTN2 | PIN_GPIO_OUTPUT_DIS | PIN_INPUT_EN | PIN_PULLUP,

PIN_TERMINATE
};

PIN_State keyPins;
PIN_Handle hKeyPins;

/*********************************************************************
* PUBLIC FUNCTIONS
*/
/*********************************************************************
* @fn Board_initKeys
*
* @brief Enable interrupts for keys on GPIOs.
*
* @param appKeyCB - application key pressed callback
*
* @return none
*/
void Board_initKeys(keysPressedCB_t appKeyCB)
{
// Initialize KEY pins. Enable int after callback registered
hKeyPins = PIN_open(&keyPins, keyPinsCfg);
PIN_registerIntCb(hKeyPins, Board_keyCallback);


PIN_setConfig(hKeyPins, PIN_BM_IRQ, Board_BTN1 | PIN_IRQ_BOTHEDGES);
PIN_setConfig(hKeyPins, PIN_BM_IRQ, Board_BTN2 | PIN_IRQ_BOTHEDGES);


#ifdef POWER_SAVING
//Enable wakeup

PIN_setConfig(hKeyPins, PINCC26XX_BM_WAKEUP, Board_BTN1 | PINCC26XX_WAKEUP_NEGEDGE);
PIN_setConfig(hKeyPins, PINCC26XX_BM_WAKEUP, Board_BTN2 | PINCC26XX_WAKEUP_NEGEDGE);

#endif //POWER_SAVING

// Setup keycallback for keys
Util_constructClock(&keyChangeClock, Board_keyChangeHandler,
KEY_DEBOUNCE_TIMEOUT, 0, false, 0);

// Set the application callback
appKeyChangeHandler = appKeyCB;
}

/*********************************************************************
* @fn Board_keyCallback
*
* @brief Interrupt handler for Keys
*
* @param none
*
* @return none
*/
static void Board_keyCallback(PIN_Handle hPin, PIN_Id pinId)
{
keysPressed = 0;

if ( PIN_getInputValue(Board_BTN1) == 0 )
{
keysPressed |= KEY_UP;
}

if ( PIN_getInputValue(Board_BTN2) == 0 )
{
keysPressed |= KEY_DOWN;
}


Util_startClock(&keyChangeClock);
}

/*********************************************************************
* @fn Board_keyChangeHandler
*
* @brief Handler for key change
*
* @param UArg a0 - ignored
*
* @return none
*/
static void Board_keyChangeHandler(UArg a0)
{
if (appKeyChangeHandler != NULL)
{
// Notify the application
(*appKeyChangeHandler)(keysPressed);
}
}
/*********************************************************************
*********************************************************************/

应用层调用函数如下:

/*********************************************************************
* @fn SimpleBLEPeripheral_handleKeys
*
* @brief Handles all key events for this device.
*
* @param keys - bit field for key events. Valid entries:
* KEY_LEFT
* KEY_RIGHT
*
* @return none
*/
static void SimpleBLEPeripheral_handleKeys(uint8_t keys)
{
uint8_t initialAdvertEnable;
if (keys & KEY_UP)
{

if (PIN_getInputValue(Board_PIN_BUTTON0) == 0)
{
initialAdvertEnable = TRUE;
// Set the Peripheral GAPRole Parameters
GAPRole_SetParameter(GAPROLE_ADVERT_ENABLED, sizeof(uint8_t),
&initialAdvertEnable);
}
}
else if (keys & KEY_DOWN)
{

if (PIN_getInputValue(Board_PIN_BUTTON1) == 0)
{

initialAdvertEnable = FALSE;
// Set the Peripheral GAPRole Parameters
GAPRole_SetParameter(GAPROLE_ADVERT_ENABLED, sizeof(uint8_t),
&initialAdvertEnable);

}
}
}

问题如下;

刚烧录完这两个按键可以正常启动和关闭蓝牙。

按下复位键之后,两个按键就不能正常工作了。不能唤醒。

请问下这是怎么回事呢?谢谢!

  • 初始化中的程序改过吗,复位后debug看程序能到这里吗
  • 没改过,初始化时是打开蓝牙,复位之后蓝牙也不能打开。
  • /*********************************************************************
    * @fn SimpleBLEPeripheral_init
    *
    * @brief Called during initialization and contains application
    * specific initialization (ie. hardware initialization/setup,
    * table initialization, power up notification, etc), and
    * profile initialization/setup.
    *
    * @param None.
    *
    * @return None.
    */
    static void SimpleBLEPeripheral_init(void)
    {
    // ******************************************************************
    // N0 STACK API CALLS CAN OCCUR BEFORE THIS CALL TO ICall_registerApp
    // ******************************************************************
    // Register the current thread as an ICall dispatcher application
    // so that the application can send and receive messages.
    ICall_registerApp(&selfEntity, &syncEvent);

    #ifdef USE_RCOSC
    RCOSC_enableCalibration();
    #endif // USE_RCOSC

    #if defined( USE_FPGA )
    // configure RF Core SMI Data Link
    IOCPortConfigureSet(IOID_12, IOC_PORT_RFC_GPO0, IOC_STD_OUTPUT);
    IOCPortConfigureSet(IOID_11, IOC_PORT_RFC_GPI0, IOC_STD_INPUT);

    // configure RF Core SMI Command Link
    IOCPortConfigureSet(IOID_10, IOC_IOCFG0_PORT_ID_RFC_SMI_CL_OUT, IOC_STD_OUTPUT);
    IOCPortConfigureSet(IOID_9, IOC_IOCFG0_PORT_ID_RFC_SMI_CL_IN, IOC_STD_INPUT);

    // configure RF Core tracer IO
    IOCPortConfigureSet(IOID_8, IOC_PORT_RFC_TRC, IOC_STD_OUTPUT);
    #else // !USE_FPGA
    #if defined( DEBUG_SW_TRACE )
    // configure RF Core tracer IO
    IOCPortConfigureSet(IOID_8, IOC_PORT_RFC_TRC, IOC_STD_OUTPUT | IOC_CURRENT_4MA | IOC_SLEW_ENABLE);
    #endif // DEBUG_SW_TRACE
    #endif // USE_FPGA

    // Create an RTOS queue for message from profile to be sent to app.
    appMsgQueue = Util_constructQueue(&appMsg);

    // Create one-shot clocks for internal periodic events.
    Util_constructClock(&periodicClock, SimpleBLEPeripheral_clockHandler,
    SBP_PERIODIC_EVT_PERIOD, 0, false, SBP_PERIODIC_EVT);

    dispHandle = Display_open(SBP_DISPLAY_TYPE, NULL);

    // Set GAP Parameters: After a connection was established, delay in seconds
    // before sending when GAPRole_SetParameter(GAPROLE_PARAM_UPDATE_ENABLE,...)
    // uses GAPROLE_LINK_PARAM_UPDATE_INITIATE_BOTH_PARAMS or
    // GAPROLE_LINK_PARAM_UPDATE_INITIATE_APP_PARAMS
    // For current defaults, this has no effect.
    GAP_SetParamValue(TGAP_CONN_PAUSE_PERIPHERAL, DEFAULT_CONN_PAUSE_PERIPHERAL);

    // Setup the Peripheral GAPRole Profile. For more information see the User's Guide:
    // software-dl.ti.com/.../gaprole.html
    {
    // Device starts advertising upon initialization of GAP
    uint8_t initialAdvertEnable = TRUE;

    // By setting this to zero, the device will go into the waiting state after
    // being discoverable for 30.72 second, and will not being advertising again
    // until re-enabled by the application
    uint16_t advertOffTime = 0;

    uint8_t enableUpdateRequest = DEFAULT_ENABLE_UPDATE_REQUEST;
    uint16_t desiredMinInterval = DEFAULT_DESIRED_MIN_CONN_INTERVAL;
    uint16_t desiredMaxInterval = DEFAULT_DESIRED_MAX_CONN_INTERVAL;
    uint16_t desiredSlaveLatency = DEFAULT_DESIRED_SLAVE_LATENCY;
    uint16_t desiredConnTimeout = DEFAULT_DESIRED_CONN_TIMEOUT;

    // Set the Peripheral GAPRole Parameters
    GAPRole_SetParameter(GAPROLE_ADVERT_ENABLED, sizeof(uint8_t),
    &initialAdvertEnable);
    GAPRole_SetParameter(GAPROLE_ADVERT_OFF_TIME, sizeof(uint16_t),
    &advertOffTime);

    GAPRole_SetParameter(GAPROLE_SCAN_RSP_DATA, sizeof(scanRspData),
    scanRspData);
    GAPRole_SetParameter(GAPROLE_ADVERT_DATA, sizeof(advertData), advertData);

    GAPRole_SetParameter(GAPROLE_PARAM_UPDATE_ENABLE, sizeof(uint8_t),
    &enableUpdateRequest);
    GAPRole_SetParameter(GAPROLE_MIN_CONN_INTERVAL, sizeof(uint16_t),
    &desiredMinInterval);
    GAPRole_SetParameter(GAPROLE_MAX_CONN_INTERVAL, sizeof(uint16_t),
    &desiredMaxInterval);
    GAPRole_SetParameter(GAPROLE_SLAVE_LATENCY, sizeof(uint16_t),
    &desiredSlaveLatency);
    GAPRole_SetParameter(GAPROLE_TIMEOUT_MULTIPLIER, sizeof(uint16_t),
    &desiredConnTimeout);
    }

    // Set the Device Name characteristic in the GAP GATT Service
    // For more information, see the section in the User's Guide:
    // software-dl.ti.com/.../gaprole.html
    GGS_SetParameter(GGS_DEVICE_NAME_ATT, GAP_DEVICE_NAME_LEN, attDeviceName);

    // Set GAP Parameters to set the advertising interval
    // For more information, see the GAP section of the User's Guide:
    // software-dl.ti.com/.../gatt.html
    {
    // Use the same interval for general and limited advertising.
    // Note that only general advertising will occur based on the above configuration
    uint16_t advInt = DEFAULT_ADVERTISING_INTERVAL;

    GAP_SetParamValue(TGAP_LIM_DISC_ADV_INT_MIN, advInt);
    GAP_SetParamValue(TGAP_LIM_DISC_ADV_INT_MAX, advInt);
    GAP_SetParamValue(TGAP_GEN_DISC_ADV_INT_MIN, advInt);
    GAP_SetParamValue(TGAP_GEN_DISC_ADV_INT_MAX, advInt);
    }

    // Setup the GAP Bond Manager. For more information see the section in the
    // User's Guide:
    // software-dl.ti.com/.../gapbondmngr.html
    {
    // Hard code the passkey that will be used for pairing. The GAPBondMgr will
    // use this key instead of issuing a callback to the application. This only
    // works if both sides of the connection know to use this same key at
    // compile-time.
    uint32_t passkey = 0; // passkey "000000"
    // Don't send a pairing request after connecting; the peer device must
    // initiate pairing
    uint8_t pairMode = GAPBOND_PAIRING_MODE_WAIT_FOR_REQ;
    // Use authenticated pairing: require passcode.
    uint8_t mitm = TRUE;
    // This device only has display capabilities. Therefore, it will display the
    // passcode during pairing. However, since the default passcode is being
    // used, there is no need to display anything.
    uint8_t ioCap = GAPBOND_IO_CAP_DISPLAY_ONLY;
    // Request bonding (storing long-term keys for re-encryption upon subsequent
    // connections without repairing)
    uint8_t bonding = TRUE;

    GAPBondMgr_SetParameter(GAPBOND_DEFAULT_PASSCODE, sizeof(uint32_t),
    &passkey);
    GAPBondMgr_SetParameter(GAPBOND_PAIRING_MODE, sizeof(uint8_t), &pairMode);
    GAPBondMgr_SetParameter(GAPBOND_MITM_PROTECTION, sizeof(uint8_t), &mitm);
    GAPBondMgr_SetParameter(GAPBOND_IO_CAPABILITIES, sizeof(uint8_t), &ioCap);
    GAPBondMgr_SetParameter(GAPBOND_BONDING_ENABLED, sizeof(uint8_t), &bonding);
    }

    // Initialize GATT attributes
    GGS_AddService(GATT_ALL_SERVICES); // GAP GATT Service
    GATTServApp_AddService(GATT_ALL_SERVICES); // GATT Service
    DevInfo_AddService(); // Device Information Service

    #ifndef FEATURE_OAD_ONCHIP
    SimpleProfile_AddService(GATT_ALL_SERVICES); // Simple GATT Profile
    #endif //!FEATURE_OAD_ONCHIP

    #ifdef FEATURE_OAD
    VOID OAD_addService(); // OAD Profile
    OAD_register((oadTargetCBs_t *)&simpleBLEPeripheral_oadCBs);
    hOadQ = Util_constructQueue(&oadQ);
    #endif //FEATURE_OAD

    #ifdef IMAGE_INVALIDATE
    Reset_addService();
    #endif //IMAGE_INVALIDATE


    #ifndef FEATURE_OAD_ONCHIP
    // Setup the SimpleProfile Characteristic Values
    // For more information, see the sections in the User's Guide:
    // software-dl.ti.com/.../gatt.html
    // software-dl.ti.com/.../gatt.html
    {
    uint8_t charValue1 = 1;
    uint8_t charValue2 = 2;
    uint8_t charValue3 = 3;
    uint8_t charValue4 = 4;
    uint8_t charValue5[SIMPLEPROFILE_CHAR5_LEN] = { 1, 2, 3, 4, 5 };

    SimpleProfile_SetParameter(SIMPLEPROFILE_CHAR1, sizeof(uint8_t),
    &charValue1);
    SimpleProfile_SetParameter(SIMPLEPROFILE_CHAR2, sizeof(uint8_t),
    &charValue2);
    SimpleProfile_SetParameter(SIMPLEPROFILE_CHAR3, sizeof(uint8_t),
    &charValue3);
    SimpleProfile_SetParameter(SIMPLEPROFILE_CHAR4, sizeof(uint8_t),
    &charValue4);
    SimpleProfile_SetParameter(SIMPLEPROFILE_CHAR5, SIMPLEPROFILE_CHAR5_LEN,
    charValue5);
    }

    // Register callback with SimpleGATTprofile
    SimpleProfile_RegisterAppCBs(&SimpleBLEPeripheral_simpleProfileCBs);
    #endif //!FEATURE_OAD_ONCHIP

    // Start Bond Manager and register callback
    VOID GAPBondMgr_Register(&simpleBLEPeripheral_BondMgrCBs);

    // Register with GAP for HCI/Host messages. This is needed to receive HCI
    // events. For more information, see the section in the User's Guide:
    // software-dl.ti.com/.../hci.html
    GAP_RegisterForMsgs(selfEntity);

    // Register for GATT local events and ATT Responses pending for transmission
    GATT_RegisterForMsgs(selfEntity);

    // Set default values for Data Length Extension
    // This should be included only if Extended Data Length Feature is enabled
    // in build_config.opt in stack project.
    {
    //Set initial values to maximum, RX is set to max. by default(251 octets, 2120us)
    #define APP_SUGGESTED_PDU_SIZE 251 //default is 27 octets(TX)
    #define APP_SUGGESTED_TX_TIME 2120 //default is 328us(TX)

    // This API is documented in hci.h
    // See BLE5-Stack User's Guide for information on using this command:
    // software-dl.ti.com/.../data-length-extensions.html
    // HCI_LE_WriteSuggestedDefaultDataLenCmd(APP_SUGGESTED_PDU_SIZE, APP_SUGGESTED_TX_TIME);
    }

    #if defined (BLE_V42_FEATURES) && (BLE_V42_FEATURES & PRIVACY_1_2_CFG)
    // Initialize GATT Client
    GATT_InitClient();

    // This line masks the Resolvable Private Address Only (RPAO) Characteristic
    // in the GAP GATT Server from being detected by remote devices. This value
    // cannot be toggled without power cycling but should remain consistent across
    // power-cycles. Removing this command when Privacy is used will cause this
    // device to be treated in Network Privacy Mode by bonded devices - this means
    // that after disconnecting they will not respond to this device's PDUs which
    // contain its Identity Address.
    // Devices wanting to use Network Privacy Mode with other BT5 devices, this
    // line should be commented out.
    GGS_SetParamValue(GGS_DISABLE_RPAO_CHARACTERISTIC);
    #endif // BLE_V42_FEATURES & PRIVACY_1_2_CFG

    #if !defined(Display_DISABLE_ALL)
    // Set the title of the main menu
    #if defined FEATURE_OAD
    #if defined (HAL_IMAGE_A)
    TBM_SET_TITLE(&sbpMenuMain, "BLE Peripheral A");
    #else
    TBM_SET_TITLE(&sbpMenuMain, "BLE Peripheral B");
    #endif // HAL_IMAGE_A
    #else
    TBM_SET_TITLE(&sbpMenuMain, "BLE Peripheral");
    #endif // FEATURE_OAD

    // Initialize Two-Button Menu module
    tbm_setItemStatus(&sbpMenuMain, TBM_ITEM_NONE, TBM_ITEM_ALL);
    tbm_initTwoBtnMenu(dispHandle, &sbpMenuMain, 3, NULL);

    // Init key debouncer

    #endif // !Display_DISABLE_ALL
    Board_initKeys(SimpleBLEPeripheral_keyChangeHandler);
    #if !defined (USE_LL_CONN_PARAM_UPDATE)
    // Get the currently set local supported LE features
    // The will result in a HCI_LE_READ_LOCAL_SUPPORTED_FEATURES event that
    // will get received in the main task processing loop. At this point,
    // feature bits can be set / cleared and the features can be updated.
    HCI_LE_ReadLocalSupportedFeaturesCmd();
    #endif // !defined (USE_LL_CONN_PARAM_UPDATE)

    // Start the GAPRole
    VOID GAPRole_StartDevice(&SimpleBLEPeripheral_gapRoleCBs);

    }
  • 复位后程序应该从头执行,不会搜不到广播,复位后单步运行看可以执行到哪一步