请问CC2640R2F的ADC例程中参考电压是多少?如果我要改为4.3V的话要怎么改呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
0: Fixed reference = 4.3V
1: Relative reference = VDDS
/*!
* @brief Specifies whether the internal reference of the ADC is sourced from the battery voltage or a fixed internal source.
*
* - In practice, using the internal fixed voltage reference sets the upper range of the ADC to a fixed value. That value is 4.3V with
* input scaling enabled and ~1.4785V with input scaling disabled. In this mode, the output is a function of the input voltage multiplied
* by the resolution in alternatives (not bits) divided by the upper voltage range of the ADC. Output = Input (V) * 2^12 / (ADC range (V))
*
* - Using VDDS as a reference scales the upper range of the ADC with the battery voltage. As the battery depletes and its voltage drops, so does
* the range of the ADC. This is helpful when measuring signals that are generated relative to the battery voltage. In this mode, the output is
* a function of the input voltage multiplied by the resolution in alternatives (not bits) divided by VDDS multiplied by a scaling factor derived
* from the input scaling. Output = Input (V) * 2^12 / (VDDS (V) * Scaling factor), where the scaling factor is ~1.4785/4.3 for input scaling
* disabled and 1 for input scaling enabled.
*
* @note The actual reference values are slightly different for each device and are higher than the values specified above. This gain is saved in
* the FCFG. The function ::ADC_convertToMicroVolts() must be used to derive actual voltage values. Do not attempt to compare raw values
* between devices or derive a voltage from them yourself. The results of doing so will only be approximately correct.
*
* @warning Even though the upper voltage range of the ADC is 4.3 volts in fixed mode with input scaling enabled, the input should never exceed
* VDDS as per the data sheet.
*/
typedef enum ADCCC26XX_Reference_Source {
ADCCC26XX_FIXED_REFERENCE = AUXADC_REF_FIXED,
ADCCC26XX_VDDS_REFERENCE = AUXADC_REF_VDDS_REL
} ADCCC26XX_Reference_Source;
和枚举中的顺序对应就可以了,例如:改为DIO25
在Board.h中
#define Board_ADC1 CC2640R2_LAUNCHXL_ADC2
/*!
* @def CC2640R2_LAUNCHXL_ADCName
* @brief Enum of ADCs
*/
typedef enum CC2640R2_LAUNCHXL_ADCName {
CC2640R2_LAUNCHXL_ADC0 = 0,
CC2640R2_LAUNCHXL_ADC1,
CC2640R2_LAUNCHXL_ADC2,
CC2640R2_LAUNCHXL_ADC3,
CC2640R2_LAUNCHXL_ADC4,
CC2640R2_LAUNCHXL_ADC5,
CC2640R2_LAUNCHXL_ADC6,
CC2640R2_LAUNCHXL_ADC7,
CC2640R2_LAUNCHXL_ADCDCOUPL,
CC2640R2_LAUNCHXL_ADCVSS,
CC2640R2_LAUNCHXL_ADCVDDS,
CC2640R2_LAUNCHXL_ADCCOUNT
} CC2640R2_LAUNCHXL_ADCName;把CC2640R2_LAUNCHXL_DIO24_ANALOG的adcCompBInput 改成ADC_COMPB_IN_AUXIO7,CC2640R2_LAUNCHXL_DIO23_ANALOG的adcCompBInput 改成ADC_COMPB_IN_AUXIO6,就可以把ADC0的腳位換成DIO24了,其他的可以以此類推
const ADCCC26XX_HWAttrs adcCC26xxHWAttrs[CC2640R2_LAUNCHXL_ADCCOUNT] = {
{
.adcDIO = CC2640R2_LAUNCHXL_DIO23_ANALOG,
.adcCompBInput = ADC_COMPB_IN_AUXIO6,
.refSource = ADCCC26XX_FIXED_REFERENCE,
.samplingDuration = ADCCC26XX_SAMPLING_DURATION_2P7_US,
.inputScalingEnabled = true,
.triggerSource = ADCCC26XX_TRIGGER_MANUAL,
.returnAdjustedVal = false
},
{
.adcDIO = CC2640R2_LAUNCHXL_DIO24_ANALOG,
.adcCompBInput = ADC_COMPB_IN_AUXIO7,
.refSource = ADCCC26XX_FIXED_REFERENCE,
.samplingDuration = ADCCC26XX_SAMPLING_DURATION_2P7_US,
.inputScalingEnabled = true,
.triggerSource = ADCCC26XX_TRIGGER_MANUAL,
.returnAdjustedVal = false
},
{
.adcDIO = CC2640R2_LAUNCHXL_DIO25_ANALOG,
.adcCompBInput = ADC_COMPB_IN_AUXIO5,
.refSource = ADCCC26XX_FIXED_REFERENCE,
.samplingDuration = ADCCC26XX_SAMPLING_DURATION_2P7_US,
.inputScalingEnabled = true,
.triggerSource = ADCCC26XX_TRIGGER_MANUAL,
.returnAdjustedVal = false
},
{
.adcDIO = CC2640R2_LAUNCHXL_DIO26_ANALOG,
.adcCompBInput = ADC_COMPB_IN_AUXIO4,
.refSource = ADCCC26XX_FIXED_REFERENCE,
.samplingDuration = ADCCC26XX_SAMPLING_DURATION_2P7_US,
.inputScalingEnabled = true,
.triggerSource = ADCCC26XX_TRIGGER_MANUAL,
.returnAdjustedVal = false
},
{
.adcDIO = CC2640R2_LAUNCHXL_DIO27_ANALOG,
.adcCompBInput = ADC_COMPB_IN_AUXIO3,
.refSource = ADCCC26XX_FIXED_REFERENCE,
.samplingDuration = ADCCC26XX_SAMPLING_DURATION_2P7_US,
.inputScalingEnabled = true,
.triggerSource = ADCCC26XX_TRIGGER_MANUAL,
.returnAdjustedVal = false
},
{
.adcDIO = CC2640R2_LAUNCHXL_DIO28_ANALOG,
.adcCompBInput = ADC_COMPB_IN_AUXIO2,
.refSource = ADCCC26XX_FIXED_REFERENCE,
.samplingDuration = ADCCC26XX_SAMPLING_DURATION_2P7_US,
.inputScalingEnabled = true,
.triggerSource = ADCCC26XX_TRIGGER_MANUAL,
.returnAdjustedVal = false
},
{
.adcDIO = CC2640R2_LAUNCHXL_DIO29_ANALOG,
.adcCompBInput = ADC_COMPB_IN_AUXIO1,
.refSource = ADCCC26XX_FIXED_REFERENCE,
.samplingDuration = ADCCC26XX_SAMPLING_DURATION_2P7_US,
.inputScalingEnabled = true,
.triggerSource = ADCCC26XX_TRIGGER_MANUAL,
.returnAdjustedVal = false
},
{
.adcDIO = CC2640R2_LAUNCHXL_DIO30_ANALOG,
.adcCompBInput = ADC_COMPB_IN_AUXIO0,
.refSource = ADCCC26XX_FIXED_REFERENCE,
.samplingDuration = ADCCC26XX_SAMPLING_DURATION_10P9_MS,
.inputScalingEnabled = true,
.triggerSource = ADCCC26XX_TRIGGER_MANUAL,
.returnAdjustedVal = false
},
{
.adcDIO = PIN_UNASSIGNED,
.adcCompBInput = ADC_COMPB_IN_DCOUPL,
.refSource = ADCCC26XX_FIXED_REFERENCE,
.samplingDuration = ADCCC26XX_SAMPLING_DURATION_2P7_US,
.inputScalingEnabled = true,
.triggerSource = ADCCC26XX_TRIGGER_MANUAL,
.returnAdjustedVal = false
},
{
.adcDIO = PIN_UNASSIGNED,
.adcCompBInput = ADC_COMPB_IN_VSS,
.refSource = ADCCC26XX_FIXED_REFERENCE,
.samplingDuration = ADCCC26XX_SAMPLING_DURATION_2P7_US,
.inputScalingEnabled = true,
.triggerSource = ADCCC26XX_TRIGGER_MANUAL,
.returnAdjustedVal = false
},
{
.adcDIO = PIN_UNASSIGNED,
.adcCompBInput = ADC_COMPB_IN_VDDS,
.refSource = ADCCC26XX_FIXED_REFERENCE,
.samplingDuration = ADCCC26XX_SAMPLING_DURATION_2P7_US,
.inputScalingEnabled = true,
.triggerSource = ADCCC26XX_TRIGGER_MANUAL,
.returnAdjustedVal = false
}
};