This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F+CC2592设置问题

Other Parts Discussed in Thread: CC2592, CC2650, CC2640R2F

除了GPIO:PA LNA HGM三个配置以外。

我看到tidub71-TIDC-CC2650-CC2592-EMK.pdf这个文档有这样的描述:

Output Power Programming
The RF output power of the CC2650 - CC2592 EM is controlled by txPower parameter on CC2650 radio setup operation. Table 4
shows the typical output power and current consumption for the recommended power settings. The value specified in the table refers
to the combined value of txPower.IB and txPower.GC.
TXPOWER Power [dBm] Current [mA]
0x3F 22.0 179.8
0x1C 20.9 155.3
0x12 19.5 134.4
0x0E 18.4 119.9
0x0B 16.9 105.1
0x53 15.9 96.0
0x51 14.9 88.3

那么是不是意味着我要去配置txPower.IB and txPower.GC.,当然我看到这个配置在ble_user_config.c文件中。

问题1:能具体解释一下吗,功率的控制是通过以上这里配置的嘛?

问题2:如果是配置CC2640R2F,那么CC2640R2F是如何通过控制CC2592的发射功率的呢?

问题3:在标准0dbm发射功率时,开启高增益模式,是否可以增强接收灵敏度,如果不能,开启了,会有其他问题嘛

  • 1、是
    2、通过互相连接的几个脚控制,设置都在CC26XX端进行
    3、高增益可以提高天线辐射或接收无线信号的能力
  • thank you.
    那我需要怎么去修改ble_user_config.c中的的参数表呢。
    // Tx Power Values (Pout, IB, GC, TC)
    const txPwrVal_t TxPowerTable[] =
    { { TX_POWER_MINUS_21_DBM, GEN_TX_POWER_VAL( 0x07, 3, 0x0C ) },
    { TX_POWER_MINUS_18_DBM, GEN_TX_POWER_VAL( 0x09, 3, 0x0C ) },
    { TX_POWER_MINUS_15_DBM, GEN_TX_POWER_VAL( 0x0B, 3, 0x0C ) },
    { TX_POWER_MINUS_12_DBM, GEN_TX_POWER_VAL( 0x0B, 1, 0x14 ) },
    { TX_POWER_MINUS_9_DBM, GEN_TX_POWER_VAL( 0x0E, 1, 0x19 ) },
    { TX_POWER_MINUS_6_DBM, GEN_TX_POWER_VAL( 0x12, 1, 0x1D ) },
    { TX_POWER_MINUS_3_DBM, GEN_TX_POWER_VAL( 0x18, 1, 0x25 ) },
    { TX_POWER_0_DBM, GEN_TX_POWER_VAL( 0x21, 1, 0x31 ) },
    { TX_POWER_1_DBM, GEN_TX_POWER_VAL( 0x14, 0, 0x42 ) },
    { TX_POWER_2_DBM, GEN_TX_POWER_VAL( 0x18, 0, 0x4E ) },
    { TX_POWER_3_DBM, GEN_TX_POWER_VAL( 0x1C, 0, 0x5A ) },
    { TX_POWER_4_DBM, GEN_TX_POWER_VAL( 0x24, 0, 0x93 ) },
    { TX_POWER_5_DBM, GEN_TX_POWER_VAL( 0x30, 0, 0x93 ) } };
  • 这个表不用改,根据此表配置你需要的TX power即可
  • thank you,viki shi。根据这个配置之后,我发现+PA之后,近距离的信号更强了。但是远距离测试时,跟不加PA的相比,距离几乎是一样的。