This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于SIMPLELINK-CC13X2-26X2-SDK_4.30.00.54和SIMPLELINK-CC13X2-26X2-SDK_4.40.04.04的区别

Other Parts Discussed in Thread: SIMPLELINK-CC13X2-26X2-SDK, SYSCONFIG, CC1352P, CC2652P

各位论坛前辈好!我想请问一下SIMPLELINK-CC13X2-26X2-SDK_4.30.00.54和SIMPLELINK-CC13X2-26X2-SDK_4.40.04.04这两个版本的SDK有什么区别,我用CC26X2R1搭载天线板做定位实验时,使用SIMPLELINK-CC13X2-26X2-SDK_4.30.00.54版本时,UI界面正常使用,但是当使用SIMPLELINK-CC13X2-26X2-SDK_4.40.04.04版本时,UI界面不能正常使用,还请各位前辈抽出宝贵时间帮忙解答一下,谢谢。

  • user6565084 说:
    我想请问一下SIMPLELINK-CC13X2-26X2-SDK_4.30.00.54和SIMPLELINK-CC13X2-26X2-SDK_4.40.04.04这两个版本的SDK有什么区别

    您可以看一下 该链接 内的 来查看区别

    此链接 是说明 SIMPLELINK-CC13X2-26X2-SDK_4.40.04.04 版本的已知问题:

    其中提到: 

    • TI Utils Execution Graph feature is added in SysConfig but it not ready for customer use

    Known Issues

    • TI Utils Execution Graph feature is added in SysConfig but it not ready for customer use
    • For CC1352P and CC2652P, there is as much as a 3 dB difference in expected vs. actual TX power. For more information see the Hardware Design app note.
    • There is an issue when using the IAR CLI tool with SysConfig. If the IAR CLI tool needs to be used, avoid the Clean command.
    • For all SDK components, the importing of IAR projects through dev.ti.com is currently not supported
    • Refer to the Document Overview for known issues and limitations as published in each SDK component’s release notes