This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: 私有协议建立无线组网

Part Number: CC2640R2F

使用私有协议开发CC2640R2F芯片,不基于蓝牙协议,只利用射频进行无线通信,建立一主多从的无线网络,采用时分复用方式,时隙间隔2ms,最大传输字节140Byte。

请问:1.RF启动接收/发送的时间大致多久?

2.RF从接收到发送再接收,反复切换是否会占用时间?若占用,大概需要多久?

3.数据写入缓存、从缓存中读取数据 两个操作有冲突吗?

4.采用私有协议,RFsetup 配置为RfSetup_R2HSM模式,无线通信码速率是否达到2Mbps?

初次学习,请求指教,谢谢~