This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: 自动和手动都无法安装XDS110 Class Application/User UART驱动,无法使用virtual UART输出信息

Part Number: LAUNCHXL-CC26X2R1

你好,

        我的主机系统为windows7,EVB型号为:LAUNCHXL-CC26X2R1。

         将串口连接到PC时,自动安装了XDS110驱动,如图1所示。使用TI的flash programmer、smart studio 7、CCS10都可以识别,可以调试。

         但是没有进一步安装XDS Class Application/User UART驱动,导致我无法交互UART信息,无法使用Btool工具。

          我尝试了设备管理器中对XDS110 (03.00.00.15) Embed with CMSIS-DAP手动安装驱动,驱动目录选择了D:\ti\ccs1031\ccs\ccs_base\emulation\windows\xds110_drivers结果无法安装,信息如图2、3所示。

         该如何解决此问题?

祝,好!